Satellite L555D-S7930

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

SEXYYY!!!!

POSTED BY: Gwyfer43 , Houston, TX
Overall rating: 5 out of 5 5 out of 5

great laptop, this laptop is a ALL-PURPOSE LAPTOP, not really used for gaming but since it's a multi=purpose laptop i use it anyways. one disavantage is the speakers, they're pretty low.

Best Buy - features & build quality

POSTED BY: Gusser , Largo, FL
Overall rating: 5 out of 5 5 out of 5

AMD Turion II Dual Core processor is plenty fast, as good as Intel Pent. Dual Core, so speedy this one is. Great machine with enough features to replace this for my desktop system. Excellent physical design, the piano black will finger print easily, but oh so pretty. Wipe it down, some complain about the slippery keys, they do take some getting used to, but I use an elevated laptop base with built in fan so hand posture is a necessity for heavy typing on any laptop. This laptop runs much cooler than the Acer I replaced this with. At 17" and setting the screen/font size to 125% this is as good of a view as a desktop for sure. I am very pleased, and the speakers have very decent volume, I compared this to an HP / MS I /ASUS / DELL, for price, featues, build quality you cannot go wrong. Yes the AMD versions are about $100 less than Intel, but that has been forever, AMD is speedy, runs PhotoShop very well.

5 Star

POSTED BY: tommy , amarillo, TX
Overall rating: 5 out of 5 5 out of 5

The big key board and the big screen is wonderful for a persons ease of seeing and typing total operation is simple and great.tommy

Very good product for the price

POSTED BY: golf man , Clearwater,Fl
Overall rating: 5 out of 5 5 out of 5

Just one bad thing...way to short witn only 2 usb ports.... And the finish of the keyboard is a fingerprint magnet the FBI will be prood of......

GREAT

POSTED BY: Jim , San Antonio,TX
Overall rating: 5 out of 5 5 out of 5

great computer and does just what I want. Heads above my old Dell

Major upgrade in a laptop

POSTED BY: klehar , Idaho
Overall rating: 5 out of 5 5 out of 5

My old laptop was getting getting to be victim of old age, especially in computer years. I am enjoying getting to know its features and learning how to navigate the new product. It was a Christmas gift and a great one at that.

Laptop

POSTED BY: HayNay76 , Harveyville, Ks
Overall rating: 5 out of 5 5 out of 5

Toshiba is the best computer I have ever owned! My only concern with it is that the battery does not last long and sometimes the performance can be a little slow. Overall though I will keep buying Toshiba!

A very good laptop!

POSTED BY: fcrooster , Fort Collins, CO
Overall rating: 5 out of 5 5 out of 5

A close friend said he loved his Toshiba, so based on that, I purchased mine. I'm still learning my way around my new laptop, but I especially like the User's Guide that helps me.

Great Laptop

POSTED BY: laptopuser1 , Calhoun, GA
Overall rating: 5 out of 5 5 out of 5

This is a great laptop. I have had no problems with it at all. Love the black color even though it does show every fingerprint.

is above other laptops

POSTED BY: tom
Overall rating: 5 out of 5 5 out of 5

is an outstanding laptop,for price and users availability is wonderful

i like this laptop

POSTED BY: doom2001 , 505 east frist st
Overall rating: 5 out of 5 5 out of 5

it can play shayia and PW and la tale and quake 2 and quake 3 and halo works fine like this laptop becuase it has a good video card better than my old laptop i cant play PW at all and shayia as well

First Laptop

POSTED BY: Cookie , Elgin,IL
Overall rating: 5 out of 5 5 out of 5

This is my first laptop and I could not be happier. Love the large screen and the keyboard. It takes no to be up and running with Windows 7. Only regret is battery life.

it is now realy a gaming laptop but it plays ok

POSTED BY: doom2009 , moscow idaho
Overall rating: 5 out of 5 5 out of 5

i play old games fine that is pretty much i focus on any way just run old game pretty much like Jedi knight out cast 2 and quake 2 and quake 3 and doom doom and doom 2 pretty much it is pretty fast it has 4gigs of ram to speed it up

Great Laptop For The Money

POSTED BY: magicguy , Murfreesboro, CA
Overall rating: 5 out of 5 5 out of 5

I bought this Laptop to replace a Dell 17 inch laptop. This Toshiba laptop is a great computer for the money. Much cheaper than what I paid for my old Dell. I like the fact that the speakers are on top and not on the bottom like most laptops. Much easier to hear the sound. Don't let the size fool you. It does not weights much. The 17" screen size is very sharp and nice. It comes with everything that generaly is needed this days. Has 2 USB ports and a media reader for the memory cards for the digital camera. It is great that it also comes with a built in web cam and microphone. It is my first computer that I have with a web cam and microphone. The only thing that can use improvement is for the battery life to last longer. Other than that, everything is great.

POSTED BY: Juju , Atlanta, GA
Overall rating: 5 out of 5 5 out of 5

Easy to use. Easy to read. One thing I would change would be to add more USB ports.

I Love My New Laptop

POSTED BY: MO , Lake Worth, FL
Overall rating: 5 out of 5 5 out of 5

I received my laptop as a Christmas gift from my Husband. I just love how easy it was to set it up and how easy it is to use. Everything was explained in step by step instructions. And within 45 minutes I was surfing the web.

Great Laptop For A Great Price.

POSTED BY: Big Al , Denver,CO
Overall rating: 5 out of 5 5 out of 5

This laptop is a terrific buy and has lots of features.The is a Skype ready webcam,a built in SD card slot for quick and easy photo downloads,wi fi that works quickly and a reasonably long battery life.I wish I had bought this computer earlier.

Pretty great!

POSTED BY: ToshibaLover
Overall rating: 5 out of 5 5 out of 5

I got this laptop for Christmas and i love it! The few things they could change is the battery life. It lasts about 2 hours, which is ok for what i use it for but it's very sad when i have to plug it in every 2 hours. Also the keys seem kind of cheap but they are still good but very thin, & also i wish Microsoft Office was not a trial, if you pay this much for a laptop it should come with the software not just a trial. Overall i am very pleased with this laptop and am very happy with the price. Couldn't have bought a better laptop.

Better than my Sony Vaio!

POSTED BY: Popeye , Lexington, KY
Overall rating: 5 out of 5 5 out of 5

We purchased the L555D at Christmas time as a gift to ourselves after purchasing one for our daughter for her present. We are very pleased with it! It operates above and beyond my Vaio ever did. The price was 1/3 that of the Sony, too!

L555D-S7930 Laptop

POSTED BY: Ebandit_64 , Lafayette, LA
Overall rating: 5 out of 5 5 out of 5

Great Value, Awesome screen

HP COMPATIBILTY

POSTED BY: TONY , CHARLESTON SC
Overall rating: 4 out of 5 4 out of 5

I BOUGHT TODAY : - A NEW LAPTOP TOSHIBA SATELLITE L555DS7930 LOADED WITH MICROSOFT WINDOWS 7 A NEW HP PRINTER OFFICEJET J4580 I WAS UNABLE TO FIND A PRINTER DRIVER ON THE DISC SUPPLIED NOR ON THE WEB WHERE CAN I FIND A PRINTER DRIVER FOR WINDOWS 7 ?

good lap top

POSTED BY: susej7019 , lindenwold nj
Overall rating: 4 out of 5 4 out of 5

toshiba is the best laptop why you make a desk top you will kink but tosiba good brand and japan best

nice laptop

POSTED BY: Dizzy , pittsburgh,PA
Overall rating: 4 out of 5 4 out of 5

I Love the large screen and keyboard. The mouse is the only issue. ii turned tapping off because there wasn't an adjustment and i kept opening things i didn't want. All in all a nice tool for the things i do surf, e-mail, bills etc. I don't game or have a need for high power

Happy with purchase

POSTED BY: Me2 , Honolulu, HI
Overall rating: 4 out of 5 4 out of 5

Battery life could be better

Love it!

POSTED BY: Capn Chaos , minnesota
Overall rating: 4 out of 5 4 out of 5

speed is great, easy to use, large keyboard, number pad!, Massive screen, battery lasts forever even while watching movies or playing games its lasted me 2 hrs. downsides: only 2 USB ports, but used properly its alright. the Toshiba keyboard KB2218 has two usb ports on it which allows one to optimize the minimal usb ports. the Touch pad is in a moderately awkward spot, sometimes when typing your hand will be touching the touch pad and move the mouse.

Decent Laptp

POSTED BY: Cortney , Middletown,DE
Overall rating: 4 out of 5 4 out of 5

I received this laptap on christmas and was very excited it's a very good laptop, the battery life is poor. If i unplug the cord for the battery out of the computer the battery only last and hour and a half to two hours depending on what you do. Although the battery life is poor i would recommend this laptop to anyone. I would also recommend a carrying case for it when you travel. Considering how wide the laptop is and how much it weighs (not that much but considering) I have not dropped it... and dont plan to and i've only had it less than a week so im not positive on how durable it is but it seems like a solid legit laptop.

Good Value

POSTED BY: shoegirl , San Pedro, CA
Overall rating: 4 out of 5 4 out of 5

I bought this to replace an HP that had more features, but I am very impressed and am happy with my purchase. Keyboard did take a moment to get used to and love that it runs so quietly. Windows 7 is excellent!

POSTED BY: you don't need to know , Oklahoma City,Ok
Overall rating: 4 out of 5 4 out of 5

It is very good operating notebook. I have enjoyed using it

ALMOST perfect

POSTED BY: Coop
Overall rating: 4 out of 5 4 out of 5

There are only two things that I could complain about this computer. First, the keys require that you strike them with a bit more force than usual. And secondly, the speakers LOOK like they would be great and they are supposed to have a great stereo sound. But even when the computer is operating optimally, the sounds quality is no better than an old AM radio. Otherwise, this a wonderfully built computer

so so

POSTED BY: MIAMI , McDonough, Ga
Overall rating: 3 out of 5 3 out of 5

I WAS TOLD BY THE SALESPERSON THAT THE AMD PROCESSOR WAS FAST, BUT IT IS NOT ANY FASTER THAT THE OLD CELERON PROCESSOR THAT I HAD ON LAST LAPTOP, WHICH WAS A TOSHIBA. I HAVE LARGE HANDS AND THE KEYBOARD LAY-OUT IS NOT FRIENDLY TO ME. SOMETIMES WHEN I'M TYPING THE CURSER JUMPS TO ANOTHER LOCATION AND I CAN'T FIGURE OUT WHAT CAUSES IT TO DO THAT.

Good Laqptop

POSTED BY: Jackmom , Texas City, TX
Overall rating: 3 out of 5 3 out of 5

Like it but have trouble with the touch pad. also seems to skip to different places and ai don't know how or what I'm doing to do that.

Not very user friendly

POSTED BY: Waldef , Kaneohe, Hawaii
Overall rating: 2 out of 5 2 out of 5

It is too heavy to carry around very long. No word processor included, or at least have not been able to find it yet! Use instructions are sketchy at best. Difficult to find battery level and memory remaining. More difficult for older users to get used to. Needs to be much more user friendly!

BAD!

POSTED BY: lapaj , garden grove Ca
Overall rating: 1 out of 5 1 out of 5

Same day I purchased worked for two hrs. Now back to repair!

TERRIBLE LAP TOP

POSTED BY: joey , wheeling il
Overall rating: 1 out of 5 1 out of 5

WORST LAPTOP I EVER OWNED

MSRP: $619.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ II Dual-Core Mobile Processor M500
  • Windows 7 Home Premium (32-bit)
  • 3GB DDR2 memory
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories