Satellite L655-S5060

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellant Value

POSTED BY: Xma223 , Columbus, OH
Overall rating: 4 out of 5 4 out of 5

Excellant performance, comfort, and reliability so far. The only issues I have so far are the speakers are very weak, and the keyboard is not back lit. Very difficult to type in low light situations, but that doesn't affect me that often. All in all this has been a great value and I would recommend it to a friend.

Should have learned the 1st time.

POSTED BY: catz , Syracuse NY
Overall rating: 3 out of 5 3 out of 5

This is my 2nd Satellite. My 1st one was ruined by my 8 yr old son in just over 1 year. Now I'm starting to wonder if it was him, or just a poor laptop. I am a huge music fan, and the volume on this thing is terrible!!! Also, the 1st time I used the disc drive to install Norton, the think made a cranking noise that almost blew me out of my chair.

MSRP: $599.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4500
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories