Satellite L755-S5308 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best for the price

POSTED BY: Nick the Greek , Englewood, Oh
Overall rating: 5 out of 5 5 out of 5

Intel I5, gives plenty of power,4G memory is sufficient for two hours average use a day. Able to project to a larger 22" monitor.

laptop

POSTED BY: val , morristown,tn
Overall rating: 5 out of 5 5 out of 5

I love my Toshiba laptop and would recommend it to anyone who wants a good computer at a reasonable price.It is also listed in the consumer report 2012 as a good computer .

Love it!

POSTED BY: Susan , Austin, TX
Overall rating: 5 out of 5 5 out of 5

I really like this laptop. It's just the right size for easy portability while the screen is still big enough to read without straining. It's fast and does everything I need.

POSTED BY: Rich , Roanoke VA
Overall rating: 5 out of 5 5 out of 5

Good Buy For The Money

just great!!

POSTED BY: eenybeany , Warwick, RI
Overall rating: 5 out of 5 5 out of 5

The Tech guy at my husband's company thought that this would be the best choice for me, and he was so right!!

AMAZING!

POSTED BY: Benlego65 , NJ
Overall rating: 5 out of 5 5 out of 5

This is a pretty good laptop. I have been using it for under a month and am loving it greatly. It is good for pretty much anything; I am fully able to play Skyrim on it with pretty good FPS (on High and Ultra!), and it also works pretty well with Ubuntu. I have yet to see any problems with it. My only complaint is the battery life; I have yet to reach 4 hours, which is quite distant from the promised 5.9 hours. Either way, this laptop is pretty amazing. Oh and also; when you are playing something, say... Skyrim, it blows A LOT of heat out; and it only exits from one area. Be careful.

My Second Toshiba - Love it!!

POSTED BY: Filly , Lakewood CO
Overall rating: 5 out of 5 5 out of 5

This laptop is very user-friendly!! My first Satellite is still an amazing laptop and is being used by my husband for his photography. My (only) two complaints are: 1) The mousepad, and 2) the battery life. 1) The mousepad thinks I want to execute a new site just because I pause. I've searched far and wide and can't find a way to turn this off. I've had to back out of many places I didn't want to go. I've learned to pause on a clear part of the screen, which isn't always convenient. At this moment, I'm using an external mouse. 2) I was told at the store that the battery life would be about 6 hours. I found 3 hours tops, which is fine. It's better than the 2 hours on the other one.

Great Laptop

POSTED BY: esdpain , Atlanta, GA
Overall rating: 5 out of 5 5 out of 5

Have laptop for i month, no problems. works great!

Amazing laptop

POSTED BY: Yiannis , Farmingdale, N.Y.
Overall rating: 5 out of 5 5 out of 5

Very pleased with my Toshiba laptop. Even though it was a present for my birthday from my wife,3 sons and their beautiful wives,I had a little something to do with selecting a " Toshiba"

Good computer...dvd drive issues

POSTED BY: Traci , gilber, az
Overall rating: 4 out of 5 4 out of 5

Purchased on 11-22-11. Easy setup. Nice computer so far. The one thing I noticed was that the dvd seems to try and read like there is a cd in it about every ten minutes. If this continues i think i might return it.

POSTED BY: Jen , Atlanta, GA
Overall rating: 4 out of 5 4 out of 5

Purchased on 11/25/1 & just like the other reviewer, I've noticed the same noise from the cd tray as well. I'm going to call customer service and if it can't be resolved I'll probably return as well. Too bad, because otherwise it seems great

good laptop for the money

POSTED BY: grayknifeart , Kansas
Overall rating: 4 out of 5 4 out of 5

Excellent laptop,fast,nice key board,love windows 7.only reason did not give it all 5 stars is DVD drive makes noise every 10 min. I keep a DVD in drive and that eliminated the noise.Can't beat the price for a powerful i5 Intel.

great so far buttttt

POSTED BY: dreggie , bethlehem,pa
Overall rating: 4 out of 5 4 out of 5

so far this laptop has been great. Im having the same problem with the cd drive just trying to read every so often even if there is nothing in the tray.. what goin on with this thing...

Excellent Value!

POSTED BY: Kirb
Overall rating: 4 out of 5 4 out of 5

This laptop is a great buy for the money. It has all of the features I need...good processor (i5), good memory (4Gig), HDMI port, and good graphics memory. The addition of Bluetooth would have been nice, but I don't really need it. I have experienced the issue with the DVD drive periodically "searching", but I don't think it's a big deal (for now).

Laptop

POSTED BY: Richi , Monterrey, NL
Overall rating: 4 out of 5 4 out of 5

Excellent laptop, very reliable, but I'm an average user that knows how to move to computers, so I do not like the laptop is the sound that makes the reproductive cd every 10 minutes and the battery capacity is too low.

Features Criticism

POSTED BY: jersey bill , Fayetteville, AR
Overall rating: 4 out of 5 4 out of 5

I would prefer to have the USB connectors located on the rear panel. It seems awkward having cables sticking out of the sidea on the laptop. I would like to have the "Volume Control" rotating knob back. Other than those two criticisms, everything else is fine.

Exceptionally Good...However CD issue

POSTED BY: Mac
Overall rating: 4 out of 5 4 out of 5

Bought on 11-25-11. Had some issues writing backup discs, and other issues with the cd drive. However this computer in my opinion is worth the money in performance and quality.

Great value!

POSTED BY: Rick , Hamburg, NY
Overall rating: 4 out of 5 4 out of 5

My second Toshiba - all the features I wanted at a price I couldn't pass up. Even though I purchased the extended warranty with my first one and never used it, I purchased it again, just in case.

DVD/CD DRIVE VFIX

POSTED BY: Fowla , Lynchburg, Va
Overall rating: 4 out of 5 4 out of 5

Uninstall Toshiba PC Health Monitor and reboot and that should fix the clicking sound every 10 minutes

average laptop

POSTED BY: Don't have one , Sahuarita, AZ
Overall rating: 3 out of 5 3 out of 5

works as expected. no wow factor found yet.

MSRP: $605.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-2430M processor
  • Windows 7 Home Premium (64-bit), SP1
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories