Satellite L755-S5357 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Value Ever

POSTED BY: Toshuser , Los Angeles, CA
Overall rating: 5 out of 5 5 out of 5

The laptop meets my expectations of Toshiba products. My only criticisms are the lack of a physical volume control and the quality of the speakers. However, to achieve the low price I realize that something must be sacrificed and these two items are probably the best choice.

Fantastic laptop

POSTED BY: tk , Long Point, IL
Overall rating: 5 out of 5 5 out of 5

This is my first laptop, as I have gone away from a desktop. What an awesome laptop for the price. Plenty of memory, good speed, and I have no doubt this computer will last me for several years.

Very good Laptop

POSTED BY: Eagle , Lubbock,Texas
Overall rating: 5 out of 5 5 out of 5

I have really in enjoyed my new toshiba laptop computer it has everything that i want in a computer.

I like Toshiba

POSTED BY: Pamala , Minneapois MN
Overall rating: 5 out of 5 5 out of 5

I would like a manual that would tell me what All the buttons do! It is a hit and miss with no manual. Why isn't a manual with this product? You are assuming that I know everything!! Thank You!

Love this laptop

POSTED BY: ladybug , Sebring, Fl.
Overall rating: 5 out of 5 5 out of 5

Have looked at a lot of laptops and for the money this is really good deal. My friends liked it so much they got one too. Good going Toshiba!!

Very Pleased

POSTED BY: Joni , West Liberty, OH
Overall rating: 5 out of 5 5 out of 5

Love my Toshiba laptop. Bought one for my daughter two years ago, and have never once had a problem with it. We will be purchasing Toshiba products only in the future.

Great Value

POSTED BY: Buckeye Dave , Napoleon, Ohio
Overall rating: 5 out of 5 5 out of 5

I feel that the L755 Laptop is a superior value for the price. Plenty of speed and memory make it a great laptop for everyday use.

Really good laptop

POSTED BY: Buddy , Lincoln, NE
Overall rating: 5 out of 5 5 out of 5

I have used several competitors laptops over the years and this is one of the best. The battery life exceeds my expectations. It boots up rapidly. The overall feel of the computer is great. I appreciate the light weight for such a large computer. I may use it for travel instead of my Netbook. My wife who uses Macs in an educational settings says this is a much better laptop. I agree

No Operating Manual

POSTED BY: Jim , Wichita, ks
Overall rating: 4 out of 5 4 out of 5

I think that Toshiba and maybe all manufacturers of computers should supply a manual to describe the function of the the controls and what they do, Shouldn't have to go to the internet to find out information

Great Laptop

POSTED BY: Daniel , Harrisburg, PA
Overall rating: 4 out of 5 4 out of 5

Very pleased with my Toshiba Laptop. I have been using it for 6 weeks with no major complaints. Easy to set up and very fast speed. The only con I have is that the speaker sounds a little tinny. Sound could be better. Besides that, great laptop!

Good Laptop

POSTED BY: zippa
Overall rating: 4 out of 5 4 out of 5

This laptop is good. I like the size of the screen and the features. I like the keys and the number pad on the side. The service is good and overall it's a great laptop. i just wish the battery life was slightly longer.

Haven't had it very long

POSTED BY: axlent , Lakewood, CA
Overall rating: 3 out of 5 3 out of 5

I really am just getting used to this laptop. I had some difficulties at first with internet connection. It would just not connect sometimes and then would start. Irritating but not horrible. Speed seems to be pretty good. Still have to spend some time learning the features, but I think it will do for now.

MSRP: $587.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2330M processor
  • Windows 7 Home Premium (64-bit), SP1
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive

shop for accessories