Satellite L755D-S5279 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great 2011 Laptop!

POSTED BY: Evans , Miami, Fl
Overall rating: 5 out of 5 5 out of 5

I'm really glad with my new Toshiba Laptop, it's all what you look for in a laptop. Pros: An amazing APU AMD proccesor, you can play at medium the most of the new games, for a integrated GPU it's impresive. I love the 15.6 widescreen LED monitor, HD videos and games look really good. Your got a strong machine for your money, the value/quality of your purchase is guaranteed. Conts: The monitor get stain easily, but you can clean it with a cotton washcloth easily to. The lid of the laptop is not as rigid as in other models, so if you carry the laptop out of a bag or briefcase, surely you will have the impression that the lid will open and close slightly.

Excelente laptop

POSTED BY: cory944 , Santa Cruz de la Sierra
Overall rating: 5 out of 5 5 out of 5

Terrific laptop, it worths every dollar, its apu is a really good combination between a processor and a video card. The video card if perfect for my needs and unless it is not a gaming laptop but you can play with good fps rate with direct x11, for the money you really get an "excelente laptop"

Great Value!

POSTED BY: Tech user , WNY
Overall rating: 4 out of 5 4 out of 5

Cheaply constructed case, but great hardware inside considering the price. Overall it's a great laptop for budget minded users looking for a very capable machine. Pros: The A6 chip is more then adequate for everyday tasks. The addition of secondary graphics acceleration is a plus. Battery life with eco mode "ON" is up to 6 hrs! Cons: Flimsy case and cheaply constructed keyboard. Real world battery life with eco mode "ON" is about 3 hours.

Great Laptop - TouchPad is tricky

Overall rating: 4 out of 5 4 out of 5

I have owned this computer for approximately three months. It exceeded my expectations - battery life was a pleasant surprise.Everything works great excerpt touch pad. Unlike on many other laptops the touch pad is not embossed into the wrist pad and for this reason it is virtually impossible to type without incidental touching of the touch pad and moving the cursor. True, there is a button above that can be used to turn touch pad off. However, this is inconvenient. I do not see why would Toshiba would do this kind of "innovation".

overall solid computer

POSTED BY: cr , il
Overall rating: 3 out of 5 3 out of 5

The A6 AMD chip is very strong at graphics processing for online games such as Battlestar Galactica online or even on video playback. The video playback suggestions for the AMD chip was really no more then 2 at a time but I was able to run 4 videos and 2 surfing apps all at teh sametime with no problem at all. My only suggestion would be to firm up the hinge more on the screen to base area. It seems looser then I would expect almost as if it was going to break but it has not as of yet so that is the good thing

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-3420M Accelerated Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories