Satellite L775-S7245 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great for the short time used!!

POSTED BY: Tinker , WI
Overall rating: 5 out of 5 5 out of 5

I am thoroughly enjoying this laptop, but cannot rate it higher at this time as I have only been able to use it for about 3 1/2 weeks.

Best laptop purchased so far

POSTED BY: cat , flat rock nc
Overall rating: 5 out of 5 5 out of 5

This is the best laptop for the money so far that i have purchased for the money. Plenty of memory and a very fast processor.

Love it!

POSTED BY: John , Rio Rico, AZ
Overall rating: 5 out of 5 5 out of 5

I have been using this laptop for a couple of weeks and it has met all my expectations. I am very happy with this purchase.

A Real Gem

POSTED BY: Dr. Hillbilly , St. Albans, WV.
Overall rating: 5 out of 5 5 out of 5

I have owned several laptops in the past ten years, and must say the Toshiba out performs all of them. I love the extended battery life feature, as well as the appearance of the machines screen resolution. The price is something that I could not pass up and fared much better than its competition.

first im pression

POSTED BY: nerd2 , omaha
Overall rating: 5 out of 5 5 out of 5

very good everything wont be disappointd

Most Bang For The Buck!

POSTED BY: HG , Gulf Breeze, Fl.
Overall rating: 5 out of 5 5 out of 5

This has got to be the best laptop purchase ever. I got more features than I could have imagined for the price I paid. It is the most stylish, professional, well built laptop ever! I have had Dell's and HP's in the past, but they didn't even come close to this one.

Great performance in short time

POSTED BY: BellaLALALA , N. Little Rock, ar
Overall rating: 5 out of 5 5 out of 5

bought this laptop for school, great value for the price, great graphics, not bad at all

great deaL

POSTED BY: jo , sparta wi
Overall rating: 4 out of 5 4 out of 5

I AM VERY HAPPY WITH MY LAP TOP

Pretty Good

POSTED BY: Missy , Redwood City, CA
Overall rating: 4 out of 5 4 out of 5

Good screen and response. Don't like the case. It is hard on the arms and rough on the edge. Keys show finger prints. USB ports would be better on the left side or exchanged with the DVD drive on the right. USB items get in the way of using the mouse.

Horrible Battery Life

POSTED BY: Lew , Jamestown, NY
Overall rating: 4 out of 5 4 out of 5

I purchased this particular Toshiba to use in the field/car. Unfortunately, the battery life is so poor that I would need a connection to a car DC outlet in order to use it for more than about 90 minutes, and that option is not available for this model, at least not that I could find on Toshiba's site. Outside of the poor battery life, this computer has been great. It's fast, has plenty of storage for my purposes, and the screen is easy to view. Two USB ports make it easy to use external devices (I recommend a mouse!), and and HDMI connection permits a direct input to my TV. A couple of other minor annoyances: the space bar, which for some reason has to be pressed on the left side or doesn't really work that well; and the touch pad, with the cursor occasionally jumping around for no apparent reason. Overall, though, I'm quite happy with the unit and would likely buy the same one again.

Not as good as I expected from a Toshiba

POSTED BY: MAS
Overall rating: 3 out of 5 3 out of 5

While the features and value seemed good with this machine, the details are not. This laptop is not up to Toshiba standards.

Powerful but sluggish

POSTED BY: calen , Pembroke Pines, FL
Overall rating: 3 out of 5 3 out of 5

Powerful and good looking laptop, but surfing the web is a little bit sluggish. When using Internet Explorer or Google Chrome pages take a while to load even when running with no add ons, very disssapointing. This is my 3rd and most powerful Toshiba laptop but the slowest in performance so far. My one year old L655 laptop runs faster with the same browser settings.

time will tell

POSTED BY: PPP , niagara falls
Overall rating: 3 out of 5 3 out of 5

This is first Toshiba computer so its a learning experience for me as we have always used HP. So far we are pleased and with more time im sure the rateing would improve

Review of Computer

POSTED BY: mailman_0 , Collinsville , Il
Overall rating: 3 out of 5 3 out of 5

nice good looking unit, worked well n fates the first 10 days, then slowed down and was hrd to figure out some of the options....not happy with the unit at all

Good, despite....

POSTED BY: BigSteve321
Overall rating: 3 out of 5 3 out of 5

My girlfriend and I picked this out because the processing speed and other tech specs seemed to dwarf that of comparably priced laptops. Everything is good so far, however after having purchased this about 3 days ago, I am already having issues with the speakers. Despite the speakers labeled as standard, there is now a horrible static noise with every sounds. Even when the volume is on low, there is still this terrible fuzzy noise emanating from each sound. I am going to schedule repairs under warranty. I will update once the problem has been resolved and what it took to get it resolved.

Not a good buy.

POSTED BY: Disappointed , Gastonia, NC
Overall rating: 1 out of 5 1 out of 5

This laptop has a lot of software issues. It has been giving me problems, since I purchased it. I would not recommend this computer.

MSRP: $679.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2310M processor
  • Windows 7 Home Premium (64-bit)
  • 6GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)