Satellite L775-S7307 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: Egyptian Diaz , San Juan, Puerto Rico
Overall rating: 5 out of 5 5 out of 5

Cool!!! I love it!!!

Love this laptop

POSTED BY: the49erhammer , Va.
Overall rating: 5 out of 5 5 out of 5

I needed a durable laptop and I found it with this one! It has more than I thought for the price. Awsome laptop!

1st laptop

POSTED BY: damar14 , No. Attleboro, MA
Overall rating: 5 out of 5 5 out of 5

it is very good, i love the camera and the quick access to the web, battery life is pretty good. can't complain about the price. so easy to use and setup

First Laptop

POSTED BY: Newbie , Hendersonville, NC
Overall rating: 5 out of 5 5 out of 5

New to the Laptop world and find this unit to be all I need.

Great purchase!

POSTED BY: travgurl , Manchester d
Overall rating: 5 out of 5 5 out of 5

Very good computer! Very happy with the performance! Great screen size!

Always a Toshiba for me

POSTED BY: Nick , Baltimore, Md.
Overall rating: 5 out of 5 5 out of 5

I have stuck with this brand , I have had a few of the others and they do not compare to this brand, It seems to me that every time I get one, It just works with no problems. this one i just purchased has a 17.3 inch screen, since i am a senior, i can see it better. also the keyboard's keys feel like a desk top keyboard, not scrunched up like a smaller laptop, it also has the keyboard with the number keys to the right like a desktop keyboard, It has a fast processor and a lot of ram, which i can expand on. I have two lap tops and a desk top, both lap tops are Toshiba, and i have bought them as a gift for my daughter and recommend this brand to others.

terrific lap top

POSTED BY: hal , stanley, nc
Overall rating: 5 out of 5 5 out of 5

i'm very happy with my toshiba. i'm an amatuer with a computer but i find this very easky to operate.

Love the laptop

POSTED BY: kat , lilburn ga
Overall rating: 5 out of 5 5 out of 5

I purchased this laptop to use for work and personal. I love the large screen and the vivid picture. I also love the fact that it is so light weight and all the features. I would definitely recommend this to a friend, actually I did. I would definitely purchase more Toshiba products in the future.

AWESOME!!!!

POSTED BY: Jay , University Place, Washington
Overall rating: 5 out of 5 5 out of 5

This is the first Laptop I have owned although I have built multiple desktops. very pleased with this laptop it is just as good as my pc. I would definitly recommend Toshiba.

Great PC

POSTED BY: Mike in Broken Arrow , Broken Arrow, OK
Overall rating: 5 out of 5 5 out of 5

This computer has everything I should ever need in a PC and at a great price. Great job by Toshiba.

Quality laptop

POSTED BY: Jon , Maine
Overall rating: 5 out of 5 5 out of 5

perfect for simple tasks....internet surfing, editting pics, etc. good product for not much $$$

Great Value

POSTED BY: dino_runs , Hollywood, Fl
Overall rating: 5 out of 5 5 out of 5

Excellent laptop at a great price...beautiful screen and easy use

darn good laptop

POSTED BY: cottonwood , Hoschton, Ga.
Overall rating: 5 out of 5 5 out of 5

I think they (Toshiba) are the best laptops you can buy. We have two in our house, one for the wife and one for me.

Good product

POSTED BY: Mattock , Newport News, VA
Overall rating: 4 out of 5 4 out of 5

I have owned 3 Toshiba laptops and loved everyone, the my lastest purchase had a problem right out of the box. I had to reload the DVD driver twice the day after I got it. Other than that its a good laptop for the money.

Great Laptop for the Money

POSTED BY: ursula531
Overall rating: 4 out of 5 4 out of 5

Performs well; but, wish the speakers were a little better! Got a great deal on the laptop; so, no complaints on pricing. Great for those looking for a secondary laptop/computer. Or, as a replacement for a desktop!

POSTED BY: baba , Surrey, BC
Overall rating: 4 out of 5 4 out of 5

It is more than worth of the price. I am very happy with its performance.

My First Laptop

POSTED BY: Mick
Overall rating: 4 out of 5 4 out of 5

This is my first laptop so still learning how to use it

No users manual!

POSTED BY: charlie , Texas
Overall rating: 4 out of 5 4 out of 5

I like my Toshiba Satellite but many of my problems would be solved if I were able to down load a users manual or at very least some thing that tells me the different key functions. So far have been unable to find a manual for my toshiba Satellite L775 on the internet. if there is a way to obtain one please advise!

great laptop

POSTED BY: jusadame , monclova coahuila
Overall rating: 3 out of 5 3 out of 5

this is a wonderfull laptop, very smooth, fast and the screen its flawless, the processor is really fast and the sound is good, the camera is awesome

Windows 7 Problems

POSTED BY: Web , maine
Overall rating: 3 out of 5 3 out of 5

Have been using this laptop for only three weeks and have had software problems twice. Had to do a compleat install of Windows 7 and hope this will hold. Laptop seems to be fine but software issues discurage me.

Had to add outside speakers

POSTED BY: T. , North Carolina
Overall rating: 3 out of 5 3 out of 5

The screen is beautiful making watching movies a real treat for a laptop. The speakers are awful, I had to plug in outside speakers. I used to own a Compaq which had speaker volume settings on the keyboard. I miss that as well as the sound system.

fist time owner

POSTED BY: bushcasade , san diego,tx
Overall rating: 3 out of 5 3 out of 5

so far I'm getting the hang of this laptop,

Very unhappy

POSTED BY: tbob58 , Grand Rapids, MI.
Overall rating: 2 out of 5 2 out of 5

Can't believe a new laptop can be so slow. Very bad picture quality for watching movies and dvd's. Worst laptop I ever owned.

worst laptop ever

POSTED BY: tbob58 , Grand Rapids, MI.
Overall rating: 1 out of 5 1 out of 5

Can't believe a new laptop can be so slow. Very poor picture quality for watching dvd's. Purchased three weeks ago and ready to throw out and replace with another brand. Total waste of money.

MSRP: $484.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor B950
  • Windows 7 Home Premium (64-bit), SP1
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)