Toshiba Satellite L855-S5155 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Windows 8 Toshiba

POSTED BY: Toots , Glendale, CA
Overall rating: 5 out of 5 5 out of 5

This is a replacement for a lower grade Toshiba, which had a problem with the mouse pad. It was only 90 days old. New one has more memory, but also costs more. I haven't gotten used to the program yet, but I can manage to do most of what I need to do

great laptop

POSTED BY: roz , Morgan hill, ca
Overall rating: 5 out of 5 5 out of 5

Love my new laptop. Other laptop was a dell

Excellent

POSTED BY: meathead , Dover, Delaware
Overall rating: 5 out of 5 5 out of 5

It has great speed, excellent screen and graphics. Great product for the price.

Good utility laptop

POSTED BY: Gokul , Pleasanton,CA
Overall rating: 5 out of 5 5 out of 5

I am glad about the purchase as all works as expected and hope Toshiba improves battery performances.

Great Laptop

POSTED BY: Grandma , Kissimmee. FL
Overall rating: 5 out of 5 5 out of 5

As far as laptops go, I have used Toshibas in the past and have alway been satisfied with their appearance, performance and value. You have a great product in a very competative market.

Would be better if...

POSTED BY: Pat , New Orleans, La
Overall rating: 4 out of 5 4 out of 5

I would happily recmmend this IF it had Windows 7 loaded on it rather than Windows 8. As it is, I will have to spend a bit of money to purchase Windows 7 and get it loaded on this laptop. The machine itaelf is great, the software preloaded is the issue.

Great, except for windows 8

POSTED BY: Ezzie
Overall rating: 4 out of 5 4 out of 5

everything is working fine. I've had some time to search the features and I have to customize to my liking. love the look of the laptop.

Expesive, but worth it.

POSTED BY: Jose , Paraguay
Overall rating: 4 out of 5 4 out of 5

It costs a little bit much taking in count another branches that have laptos with similar characteristics or better ones and are cheaper.

A perfect fit

POSTED BY: alexbas606 , Bangalore, India
Overall rating: 4 out of 5 4 out of 5

I am a student, and this being my first laptop, I actually find it really good. It does everything I need it to. It is perfectly easy to use and I hope it will last for a long time

Great laptop

POSTED BY: Motorcycler , Houston, TX
Overall rating: 4 out of 5 4 out of 5

Reliable and fast, it is perfect for day-by-day activities.

Very nice laptop

POSTED BY: Flash , Sebring, Fl
Overall rating: 4 out of 5 4 out of 5

Have a time with the windows 8, still haven't mastered that yet.

Pretty good laptop.

POSTED BY: bg , Maryland
Overall rating: 3 out of 5 3 out of 5

So far so good! Speed is respectable, it does everything well. Windows 8 -grrr, it takes a bit of getting used to. So far, no problems. Not sure about the quality of the materials, keys, shell, etc., - not quite as solid as my last laptop - guess that's how they keep the cost and weight down . Glad I got the insurance. Again, for the price, it's pretty good.

uncomfortable keyboard

POSTED BY: Dagara , Fremont
Overall rating: 3 out of 5 3 out of 5

Toshiba laptop L855-S5155 which is not at all good to use because it has 2 main disadvantages. 1.Quality: It contains very much delicated keypad. 2.Function Keys:it contains audio/video options as primary. Suggestions: Need to improve the quality of keypad. Include separate function keys line at top

Tech Issues

POSTED BY: StL , St. Louis, MO
Overall rating: 2 out of 5 2 out of 5

Having Problems, must have got a lemon... I shut it off and the systems appears to shut down but the power light and the wi-fi light stays on. The system also had a charging issue it was plugged into the wall and failed to start charging. It proceeded to run out of power and shut down. It is going to have to go back to Tech Support, wish me luck with that!

MSRP: $604.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3230M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories