Toshiba Satellite L855D-S5117 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Good laptop, my first.

POSTED BY: longbead , Florida
Overall rating: 5 out of 5 5 out of 5

This is the first laptop I've owned and I'm very pleased with the performance. I cannot compare it to anything since it is my first but so far it's great. I love the size and the keyboard.

Very good

POSTED BY: retired , Orange, CT
Overall rating: 5 out of 5 5 out of 5

Trouble with Windows 8. Are there instructions for using windows 8?.

I'm new

POSTED BY: joe , Ironwood MI
Overall rating: 5 out of 5 5 out of 5

The laptop was easy to use even though I'm am fairly new at using it. Windows 8 took a little time to get familiar with, but I'm learning to use it.

Very good laptop

POSTED BY: Josh , Perry Heights, OH
Overall rating: 5 out of 5 5 out of 5

This is a very good laptop. The processing speed is the fastest of any laptop I've ever used, and it can handle a LOT of multitasking.The only issue I have, and this is a very small issue, is that when the battery is low, it doesn't give much warning.

Best Laptop Ever

POSTED BY: NANA , Raleigh, NC
Overall rating: 5 out of 5 5 out of 5

I love the Toshiba brand Laptop. I have bought 3 over the years and would own nothing else.

Great Laptop for me

POSTED BY: Satellite , Houston, TX
Overall rating: 5 out of 5 5 out of 5

This Laptop is perfect for what I need it for. I'm an Internet Sales Manager for a Lexus dealership in Houston TX and on the computer all day every day and when I come home I need to only check emails and research topics that I like. This Laptop is perfect for what I need and it's the second Laptop from Toshiba in four years. I love it!

Love It

POSTED BY: NAPALM71 , So Cal
Overall rating: 5 out of 5 5 out of 5

Been using a satellite for years now my first one lasted for 7 years while outlasting other laptops of my friends and family so i bought another one this year and i am loving this one just as much I would definitely recommend Toshiba to ANYONE

great laptop

POSTED BY: hunter , dayton nv.
Overall rating: 5 out of 5 5 out of 5

we love our toshiba laptop thank you

GOOD LAPTOP EVER

POSTED BY: morrongo , new york .ny
Overall rating: 5 out of 5 5 out of 5

Well its a good product and Im really satificied with this product.

great laptop

POSTED BY: lindee , salisbury,maryland
Overall rating: 5 out of 5 5 out of 5

had a larger screen but like this better not as bulky

Great product at a great price

POSTED BY: Borneoclue , Elgin, IL
Overall rating: 5 out of 5 5 out of 5

We are pleasantly surprised at the quality of this product for the price. The size of screen is great, the quality of the graphics and all the extras that come with it are also good.

Toshiba has ALWAYS been good (for me)

POSTED BY: Bubbles , Hampton, VA
Overall rating: 5 out of 5 5 out of 5

I've had my Toshiba Satellite for approximately a month now. In my opinion, it's very 'user friendly'! I read many comments about the new Windows 8 & was very reluctant to get this laptop (or any other laptop with Windows 8). I have absolutely no clue what the big fuss is about. Ok, there's no actual 'Start' button to select. But, all I have to do is scroll my mouse to the bottom, left-hand corner and a small window appears that says 'START'! All of the tiles are in the 'Start' box and it's really not that hard to go through the tiles and find what you're looking for (i.e. camera, music, Netflix, etc.). And the ESC (escape) button is my friend, when exiting the start menu. I did have a moment of confusion, as far as knowing how to shut my laptop off. So, I looked up the information on Google (too easy!) If you want to open a new window and you notice other windows that you thought you exited out of, just scroll your mouse over the upper, right-hand corner of that window (without actually clicking on it) & click on the red 'x'. Sometimes, it takes more than one or two clicks to fully exit the window. I came to the conclusion that, that's because I did more than one search in that window. I'm not sure if there's a "better" way to exit a window but this way works fine for me. It gets the 'job' done! Windows 8 isn't as complicated and "scary" as some of the comments proclaimed it to be! The ONLY difference (that I'm aware of) is that all the stuff that's automatically visible on Windows 7 ('start' button, power button, tool menu, etc.) aren't automatically visible on Windows 8. But, all I have to do is either scroll my mouse to the bottom, left-hand corner or the upper, right-hand corner of my screen. I really dislike the fact that people are so quick to share negative comments about people and things that they cannot (readily) comprehend. To be calm and patient is to have understanding because anger is irrational! All that has been typed in this review is typed by someone who is almost ABSOLUTELY illiterate, when it comes to technology! (I get cell phones and mini computers confused with each other. I think the mini computers are referred to as tablets or something.) My husband usually has to teach me how to operate a lot of the functions on our televisions/remotes, how to do things on computers/laptops, how to operate the game consoles, etc. But, I figured out this Windows 8 Toshiba Satellite laptop (with God's help through a little prayer), in about an hour or less. I personally dislike the fact that technology keeps changing but it's the way of our lives in 'this day & age'. Why did I purchase a Windows 8 laptop instead of a Windows 7 laptop? Windows 8 is extremely cheaper than Windows 7!

Excellent value, Workhorse

POSTED BY: David , Charlotte, NC
Overall rating: 5 out of 5 5 out of 5

Strong processer and graphics for $ Solid computer

Very Fast Laptop

POSTED BY: Dot , Ballston Spa, NY
Overall rating: 5 out of 5 5 out of 5

I really like the exceptional speed of this laptop. No more waiting to bring up the start page, the email or favorite websites. The resolution is fantastic. The price for the speed and capacity is very good.

Excellent laptop

POSTED BY: LC , Springfield, IL
Overall rating: 5 out of 5 5 out of 5

I received this laptop for my birthday and it has been a great machine. It has the larger keyboard with the number pad that I wanted. The keyboard has a nice feel. The mouse pad works better than I expected.The only thing I wish it had was a longer battery life but I use this primarily from home anyway. I am very pleased with this laptop and would highly recommend one to my family & friends. I have always wanted a Toshiba laptop and I am very pleased.

fast laptop

POSTED BY: bigvpower
Overall rating: 5 out of 5 5 out of 5

Nice fast laptop. It has windows 8 designed for touch screens but this computer isn't a touch screen. It don't seem to make that much difference overall. This is a nice laptop, Fast and lots of disk space on the hard drive. I am loveing it.

Great laptop

POSTED BY: Troy , Phenix city, al.
Overall rating: 5 out of 5 5 out of 5

This is a great laptop for my work. I am on the road most of the time and connect through a MIFI. No issues. I did bump the RAM up to 8 gigs simply because I need a lot of windows open at the same time and my work operating software. It handles it with out a problem.

Love it!

POSTED BY: twarren , Fayetteville, NC
Overall rating: 5 out of 5 5 out of 5

Great laptop! Perfect for what I use it for. Which is mainly for Skype with the family and uploading and organizing family videos and photos. Super fast!!!

Good Laptop

POSTED BY: JimEfun , Saint Petersburg FL.
Overall rating: 5 out of 5 5 out of 5

Works great for all I do.!!!! I think it is a good buy.!!!!!!

My Laptop

POSTED BY: Pumpkin , Huxley, Iowa
Overall rating: 5 out of 5 5 out of 5

This is my first laptop, and I really like it!

Great Affordable Laptop !!!

POSTED BY: Marilyn , Forestdale, MA
Overall rating: 5 out of 5 5 out of 5

Laptop has many new features I have never seen before, like talking voice assistance. Great quality at a great price.

good basic performance,

POSTED BY: J
Overall rating: 4 out of 5 4 out of 5

lightweight, good display but speakers are a disgrace- somebody just took headphone speakers and stuck them inside, tinny, poor clarity Hate Windows 8 but had no choice

Good Value

POSTED BY: RMBH , Georgia
Overall rating: 4 out of 5 4 out of 5

Overall, I like this computer. Screen size is great. I would prefer longer space bar even if that means not having the right side numeric keys. Also, would have preferred not to have had Microsoft 8 installed. It is a challenge to learn new ways to navigate. In many cases, it has gone from one step to multiple steps to get to the final results ... e.g. printing a document.

windows 8

POSTED BY: twoshoes , newark, ohio
Overall rating: 4 out of 5 4 out of 5

still trying to get use to it

My first laptop but best one, no complaints.

POSTED BY: Nazz , Danville PA
Overall rating: 4 out of 5 4 out of 5

I use this for online school and it works great for that! Sometimes netflix, works great with that too. I would and do suggest this brand of laptop and specifically this one!

POSTED BY: Bill , Avon, New York
Overall rating: 4 out of 5 4 out of 5

I really like this computer. It meets all my current needs. I am a little confused about Windows 8 though. I cannot believe there isn't a calculator on Windows *, I had to Google it to find the calculator.

Battery Life

POSTED BY: The King , NY
Overall rating: 4 out of 5 4 out of 5

I like to have my computer on the highest brightness settings. If you could improve the life of the battery on the highest brightness the laptop would be way better.

Really Like This Laptop!!

POSTED BY: fys , Texas
Overall rating: 4 out of 5 4 out of 5

It's fast, lightweight, very affordable and user friendly (especially for a Windows 8 novice.) Even gave me a free download of Windows 8 for Dummies. :)

Good laptop.

POSTED BY: Marc
Overall rating: 4 out of 5 4 out of 5

Battery life is not that great. I am not a Windows 8 fan, do not like the start menu that well, but am getting used to it.

Just what I needed

POSTED BY: Vange , Burlington,NC
Overall rating: 4 out of 5 4 out of 5

I have been unemployed for a while now and didn't have much money to spend. But when my daughter requested that I return her computer to her I found myself without contact with my family and friends. So I went computer shopping, like most people on the web. This sweet little laptop was my dream come true. It does everything I will need to do quickly and efficiently and at a price even I could afford. Thanks Toshiba for looking out for the little guys.

BEST LAPTOP SO FAR

POSTED BY: GUNNY , TEMECULA, CA
Overall rating: 4 out of 5 4 out of 5

THIS IS THE FIRST TOSHIBA PRODUCT THAT I'VE EVER OWNED, BUT WINDOWS 8 ?... BUT I WILL GET USED TO IT. I ONLY LOOKED FOR A USER GUIDE FOR WINDOWS 8!!

POSTED BY: Christopher
Overall rating: 4 out of 5 4 out of 5

After three consecutive laptops from Toshiba, I've realized that their laptops are always affordable yet efficient. You get what you pay for without breaking your bank!

Good laptop for the money

POSTED BY: Jim , Lubbock Texas
Overall rating: 4 out of 5 4 out of 5

The Toshiba L855D-S5117 is a good value for the money . Their is only 2 problems that I personally have with it (1) Windows 8 I am a Windows 7 fan. (2) the CPU cooling vents could be a little larger to help cool it. I relay like the LED monitor it is less harsh on the eyes and is very clear and sharp. My main reason for choosing this lap top was the AMD microprocessor since I personally prefer the AMD over the other brand I have been using them for 20 years and grown to trust their reliability and performance.

Good value; great performance

POSTED BY: ToshibaReturnedUser , Canada
Overall rating: 4 out of 5 4 out of 5

The laptop works very well. The performance and expected functions work fine. A bit too many unnecessary apps and gadgets that need to be uninstalled (annoying more than anything). Otherwise, OK.

Speaker

POSTED BY: max , Ohio
Overall rating: 4 out of 5 4 out of 5

You need to replace the speaker.

Good Value Laptop

POSTED BY: RedNeck1969 , RightHereIn, FL
Overall rating: 4 out of 5 4 out of 5

This laptop is a good value for the money. If you are a student or a business person using MS Office, internet & email this will be an excellent laptop. It is even great for watching videos and Hulu. I am not a big fan of the Windows 8. It was designed for touch screens and it is a bit difficult to navigate with a mouse.

warranty

POSTED BY: Olimpo , Buenos Aires, Argentina
Overall rating: 4 out of 5 4 out of 5

I bought the product in the USA and the warranty is not covered in my country. Since the company is in my country and that the product is new. I do not clarified at the time of purchase.

Great llittle Laptop

POSTED BY: ronsco3 , Martinsburg Wv
Overall rating: 4 out of 5 4 out of 5

Everything worked great until I added some bigger un needed programs , which really slowed down performance , other then that it is a very nice Laptop ; Although it gets hot very fast which does concern me because I have no Laptop stand for it to keep cool , I will get one in the future thoufgh !

Laptop great value but monitor needs a rethink.

POSTED BY: dhatha , Knoxville, TN
Overall rating: 4 out of 5 4 out of 5

Size of keyboard, key spacing - EXCELLENT! Mousepad - more impressive with each use. Ergonomics are excellent and a big factor for someone like me who wants a notebook (larger keyboard, monitor, etc). The screen resolution is not great and when viewing from an indirect angle it gets worse quickly. I did add 8GB of RAM (now at 12GB) and that did help for overall performance including the OS of Windows 8.... which leads me back to the monitor which is not touch.

Slick

POSTED BY: PD , Beaufort, SC
Overall rating: 4 out of 5 4 out of 5

Easy to use. Upgraded to Windows 8.1. Limited apps allowed. Easy to use with plenty of help areas to go to.

A value for money laptop

POSTED BY: GautamMKGarg
Overall rating: 4 out of 5 4 out of 5

I doubt its quality.

Dependable performer

POSTED BY: dougienerd , Louisville, Ky
Overall rating: 4 out of 5 4 out of 5

Very fast-like quad core. easy interface and easy to tweek and change settings for my own convenience. fast to get on line after start-up. easy to close programs for fast shut down. Seems well constructed and stable. Only complaint-poor sound.

Just OK

POSTED BY: mdc , Michigan
Overall rating: 4 out of 5 4 out of 5

It doesn't pretend to be a high-end laptop. It does what it is supposed to. The speaker is horrible, with headphones the sound is fine. The worst thing about it is that it comes with Windows 8. What a horrible mess!

great laptop

POSTED BY: biker babe , paw paw mi
Overall rating: 4 out of 5 4 out of 5

1st quad core ive had and i love the speed and clarity. getting used to windows 8 was the hardest part of navigating.

Good laptop for the money

POSTED BY: Jim1955 , Georgia
Overall rating: 4 out of 5 4 out of 5

This computer is well built and seems sturdy. It is fairly thin and light. The performance is good with the quad-core AMD processor. Windows 8 took a little getting used to, but that is beyond the scope of this review. The computer boots quickly, and is ready to use in a few seconds. It handles the standard office tasks well and quickly. Video playback is good from sites like Youtube, etc. I have not tried the DVD drive, but have no reason to believe it would be any less than good. One quibble I do have is the speaker volume is low and it is hard to get enough signal out of it. The WiFi works well, I have an N router in the other end of the house and get reliable and speedy connections with this machine. All in all, I am happy with this computer and would recommend it to others. I would have to tell them to get a good set of earphones though.

Review on Computer

POSTED BY: Tsonata , Beaver, PA
Overall rating: 4 out of 5 4 out of 5

My overall satisfaction is good my disappointment is in the fact that there are no Microsoft products, you have to purchase Micrososft office in order to really get the computer to function on the level that I need it too. That was a big disappointment on my part. The other disappointment is that I do not like Window 8, I feel that it is hard to use and that it is not user friendly. I feel that customers should have the option of the operating system that they like or want and not be forced to take Windows 8.

Nice.

POSTED BY: DooD , Southern California
Overall rating: 4 out of 5 4 out of 5

Nice laptop. Runs everything I want it to, even a couple games. Windows 8 is a pain to get used to. The only thing I really don't like about this computer is the speakers. They don't sound very good. If I'm just surfing the net and not watching videos, the battery lasts quite a long time.

very good laptop

POSTED BY: Phil
Overall rating: 4 out of 5 4 out of 5

This laptop is everything I was hoping it would be. I've used Toshiba product for the past few years and I've always had a good experience. My only issue with my l855d s5117 is that the built in speakers are not good at all.

Keyboard is cheap

POSTED BY: Ebeeee , Rochester NY
Overall rating: 3 out of 5 3 out of 5

The keyboard is really cheap . I wish I had looked at that cloesr when I bought it & upgraded. Other than Windows 8 ( which I hate), the laptop works well.

Very Cheap

POSTED BY: JRA , Claremore, OK.
Overall rating: 3 out of 5 3 out of 5

I now wish I would have gone with my original intent to purchase a different brand of LapTop and not have listened to the salesperson in the store. I have owned Toshiba LapTops in the past and have always had good performance. This particular laptop is constructed so cheap that you can not even stand to listen to anything from the installed speakers. The sound is so bad that it is hard to even understand what is being said, sounds like the speaker is at the bottom of an old tin can. The screen definition is very poor and it is hard to distinguish between the background and the program screen. I have tried the adjustments without a real acceptable result. Needless to say I am not happy with this particular purchase. I travel for my job and did not have time to really set this laptop up until today. I actually purchased it on the 5th of May and would return it and even purchase a higher level unit, but the store in which I purchased the laptop has a 15 day exchange policy which I naturally have missed. As I stated previously I have owned Toshiba laptops in the past and have always been happy with their performance. I am not against moving up to a better grade unit from Toshiba, but I think they just cut too much quality from this laptop and it does not perform as well as lesser known units.

Replacement Laptop

POSTED BY: K O , Hot Springs, Ark.
Overall rating: 3 out of 5 3 out of 5

I bought this laptop to replace a Dell that was over 8 years old. I wanted better speed and function, but it seems the same or not as good in all functions.

I AM dissappointed

POSTED BY: nettie , charlotte nc
Overall rating: 3 out of 5 3 out of 5

Mouse/picture/lighting/copying /website switch and battery

no

POSTED BY: none , newmarket,nh
Overall rating: 3 out of 5 3 out of 5

traded from hp and im not impressed would like hp bac better gaming less problems

POSTED BY: Chris , Motown
Overall rating: 3 out of 5 3 out of 5

Windows 8 is absolutely horrible. The computer itself is OK, but I don't like the ports on the side, they should be in the back.

Good laptop

POSTED BY: Cindy , Apex, NC
Overall rating: 3 out of 5 3 out of 5

Good laptop, but don't like the windows 8 program. Very difficult to navigate. I'm sure I'll get used to it eventually.

worst speakers ever

POSTED BY: volman , ft wayne, in
Overall rating: 3 out of 5 3 out of 5

WHEN MY OLD TOSHIBA LAPTOP (8 YEARS OLD) RECENTLY DIED I CHOSE ANOTHER TOSHIBA EXPECTING THE SAME QUALITY. WAS I EVER WRONG. MY OLD SPEAKERS AND WIRELESS WERE SUPERB. THIS ONE HAS THE WORST SPEAKERS I HAVE EVER HEARD AND THE WIRELESS CARD HAS EXTREMELY SHORT RANGE. I HAD TO PURCHASE A CLIP ON SPEAKER AND AN USB WIRELESS CARD TO BRING IT UP TO MY OLD COMPUTER STANDARDS. THE COMPUTER OTHERWISE APPEARS TO WORK QUITE WELL BUT EXTREMELY DISAPPOINTED IN THESE MENTIONED FEATURES.

Good for every day

POSTED BY: Bazal , San Diego CA
Overall rating: 3 out of 5 3 out of 5

It's good tool, has all features for work.

touchy thing

POSTED BY: cakelady , fremont, nebraska
Overall rating: 3 out of 5 3 out of 5

like it, but really touchy. likes to flip between screens without my wanting to.

My laptop

POSTED BY: Blondie
Overall rating: 2 out of 5 2 out of 5

My husband and I purchased this laptop a few weeks ago, since our desktop has finally passed on. There is some problem with Internet explorer that has to stop and reload everytime there is a new page (or folder, perhaps) and then will continue. I've read a lot of similar problems online as well. I'm not real happy with it at this time. That is really my only issue tho so if that were fixed I think I'd love it

Good laptaop, poor screen

POSTED BY: Framerep , Shreveport, Louisiana
Overall rating: 2 out of 5 2 out of 5

3/4 of the screen goes white. It is obviously a fault in the workmanship or connections of the screen. I'm not happy with this product since I can't use it about 1/2 the time when I need to. This screen will not allow me to use the laptop about 80 % of the time. I need to know what I can do since I've only had the product for 5 weeks.

very difficult to use

POSTED BY: George , Montana
Overall rating: 2 out of 5 2 out of 5

This is my first lap top. I'm sorry I didn't get another pc as I find this machine very hard to get around on it. I am having a very hard time with my photos and organizing them, or even finding them. maybe a more expensive lap top is easier to use. This is not a user friendly computer.

FREEZES DAILY

POSTED BY: beth , Annapolis,MD
Overall rating: 2 out of 5 2 out of 5

PRO:The internet speed is good CONS: The mouse freezes up 4-5 times a day . To unfreeze the screen you have to hold the power button down until it shuts off. This should not be happening with a brand new computer. The speakers are about average when using headphones

POSTED BY: SAD
Overall rating: 2 out of 5 2 out of 5

do not like

No Windows 8

POSTED BY: jerryb540 , Springfield, MA
Overall rating: 2 out of 5 2 out of 5

Windows 8 is terrible and I returned the laptop.

Windows 8 ruins use experience

POSTED BY: Jxn
Overall rating: 1 out of 5 1 out of 5

Windows 8 is not a user friendly operating system and as a result the suse of the Toshiba has been made difficult with a need for work-arounds. Performing what were previously simple acts now take much longer, if it can be figured out at all. In brief my experience has been HORRIBLE-- worse than the Vista debacle.

WORST machine ever

POSTED BY: llo , St. Louis, MO
Overall rating: 1 out of 5 1 out of 5

I would never buy from Toshiba again. In fact if I could return this miserable machine for my money back I would.

Pain in the butt

POSTED BY: Unhappy Camper , Anchorage, Ak
Overall rating: 1 out of 5 1 out of 5

Windows 8 and all those horrible apps should be tossed in the trash and never seen again. This is the most difficult computer I have ever had. When AOL is opened, it is 2.5 inches in length and partly fillls the screen. When i click on the enlarge square, the width moves a lttle not the length. I havve to "pull' the lenght down to get the screen to a useable size. Howeverm when ever i change to another screen for AOL. it is right back to 2.5 lengh and I have to start the procss all over again. SO exasperating!

Don't buy.

POSTED BY: beardedcanuck , MA
Overall rating: 1 out of 5 1 out of 5

I have a couple laptops and a Toshiba Desktop as well. I am using this laptop primarily for when I travel for work. I want a bigger screen to work on than the 13" HP that I have. The Good: Price is good...not great, but not bad. The processor hums along well for most things, but I haven't tried any graphic intensive programs yet other than a few movies, word and powerpoint. That's about it. The Bad: The feel of this laptop is cheap. When I pick it up it feels like I am going to crush it. The keyboard is bad, the entire the depresses when you type. The mousepad is okay but the buttons on the mouse are loud and only work if you press them with severe force. The Ugly: The speakers are terrible. I have not heard speakers this bad on a computer or laptop since, well ever. I can't explain it, but they are absolutely terrible. They are not loud, which isn't a big deal, but the are tinny and seem to echo and just outright bad. Did you steal them off a laptop from 1995? You can't even listen to them...it is like a cat being run over by someone scraping their fingernails on a chalkboard. Terrible. The wireless adapter is ugly, it constantly drops the network and it doesn't matter which network or where I am. The screen has a terrible viewing angle and is way too dim. No matter how much brightness you add it is just terrible. And don't get me started on all the bloatware that is pre-loaded and you can't remove...waste of space and time. Overall: I am away for a month from home and can't return this piece of plastic because I left the box and manuals at home. If I had the box with me I would return it in a heartbeat. I doubt it will last a year judging by the quality of the build. Terrible cheaply made product...don't waste your time or money on this thing.

PROBLEM LAPTOP

POSTED BY: JIM
Overall rating: 1 out of 5 1 out of 5

I CAN'T READ MY E-MAIL. EVERYTIME I GO ONLINE, AFTER ABOUT ONE MINUTE IT FREEZES UP. VERY FRUSTRUATING. I WILL HAVE TO TAKE IT IN TO HAVE THEM LOOK IT OVER AND SEE WHY IT WON'T STAY ON.

Hated it

POSTED BY: none , san diego, CA
Overall rating: 1 out of 5 1 out of 5

I returned the computer. I hated the layout of the keyboard and the performance. I tried to run a powerpoint presentation with 17 MB and it said it was low on resources. That was the only program I had installed as the machine was new. I took it back and bought a Sony instead.

MSRP: $504.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A8-4500M Accelerated Processor
  • Windows 8
  • AMD® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)

shop for accessories