Toshiba Satellite L875D-S7131NR Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Awesome!

POSTED BY: Ember , SC
Overall rating: 5 out of 5 5 out of 5

This computer has it all. I absolutely love it. I'm not overly fond of windows 8. That has been horrible overcoming. I ended up using the Shell to overcome that issue. Now it works like windows 7. The performance of this computer is fast, runs nice and cool all the time. I highly recommend this computer for any gaming, even heavy gaming. It works wonderfully. The Nvidia graphics is the best around, by far.

Very nice laptop at a great price.

POSTED BY: rob , South Carolina
Overall rating: 5 out of 5 5 out of 5

I chose this laptop for it's features, large screen and great price and I am very happy with my selection. It is very quiet, fast, has good battery life and runs much cooler than my old laptop. If you want a very nice, value priced laptop or want to move from a desktop to a laptop at home, this laptop is worthy of your consideration.

Great Value

POSTED BY: Nik , St. Louis, MO
Overall rating: 4 out of 5 4 out of 5

Great value on a laptop! The HD screen is a huge plus with vivid color and pictures. I luv the trackpad and the keyboard setup including the number pad. Still trying to get used to Windows 8. The keyboard template was not installed correctly when received but the technicians where I bought it fixed it immediately. So far I'm a little dissapointed in the AMD Quad core procesor. Videos seem to load a bit slower than in Intel models even a few years older.

MSRP: $604.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A8-4500M Accelerated Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories