Satellite M305-S49052

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

I Love This Laptop

POSTED BY: LACEE54 , Northern, Virginia
Overall rating: 5 out of 5 5 out of 5

I purchased several laptops which I returned because they had something not working right. I purchased this Toshiba and it worked perfectly from the first minute. They do need to tell people that the "plug and play" doesn't work unless you go into the program and turn it on. I called Toshiba Support and they told me how to turn it on and "poof" it worked right away. I honestly can't say enough good things about this laptop to have everyone realize how nice it is!! Iove the look, the way it t ypes, it's lightweight, good battery life, awesome picture - perfect laptop. Way to go Toshiba!!

This Lap Top Is Off The Hook

POSTED BY: LatinJazzMan , NJ
Overall rating: 5 out of 5 5 out of 5

I have a desk that is great but nowhere like my laptop. It is super fast and reliable.

laptop M305-S49052

POSTED BY: lovendamouth , laurel, ms
Overall rating: 5 out of 5 5 out of 5

i have had this laptop about 9 months and it does everything that i wanted it to do. the only thing is when i bought it, the spec sheet said the motherboard was expandable to 8 gigs of ram and come to find out it is maxed out at 4. mine came with 4 gigs. i love it over all. it's great. the only other draw back is the hard drive is not sata. that is the only 2 things. i would buy another toshiba.

Very good laptop

POSTED BY: Gb , Aruba
Overall rating: 4 out of 5 4 out of 5

This laptop is very good. Only drawback is the time it takes to startup. It takes ridiculous to much time to startup. Performance is good. Batterylife is very good. I got my laptop with an extended battery. All in all i can and will recommend this laptop to a friend.

Very Good Laptop

POSTED BY: Jerry , Eagle Pass, Tx
Overall rating: 4 out of 5 4 out of 5

I like it, because have some security features that are very safe a securely, like the Face Recognition System. Very good performance and system. I hope that I can renew my Windows Vista to Seven.


POSTED BY: granny , Oregon City, Or
Overall rating: 4 out of 5 4 out of 5

Laptop, itself, is user friendly, especially for a old lady! I got rid of a bulky old computer and really like the laptop without alot of extra stuff I had to have.

Dislikes Only

POSTED BY: JeminOrbt , Titusville, FL
Overall rating: 4 out of 5 4 out of 5

Touch pad too sensitive at times. Twice typing came up gibbership, and once in reverse order. A couple of old programs will not run properly . . . maybe be a Microsoft problem. I am neither a beginner nor an expert on the pc.


Overall rating: 2 out of 5 2 out of 5

Many techincal diffuculties like the cd drive not opening and the power chord failing and the internet adapter failing, and system crashingfor no reason.

MSRP: $704.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories