Satellite M505-S4972

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Pretty happy

POSTED BY: gg , Seabrook,TX
Overall rating: 5 out of 5 5 out of 5

The laptop is great except that the air card does not work.

Good Laptop

POSTED BY: Sweetie B , Atlanta, GA
Overall rating: 4 out of 5 4 out of 5

I wish the keyboard was illuminated. The keyboard is very hard to see if you are not in a well lit area. This is my first laptop with a webcam; Skype is fun! This computer doesn't have a hibernate option, only sleep mode. Also isn't bluetooth capable. A couple features I didn't look for when I was searching for a new laptop.

Value

POSTED BY: Sweetie B , Atlanta, GA
Overall rating: 4 out of 5 4 out of 5

The keyboard is dark and needs the option of illuminating. My first laptop with a webcam, and using Skype is fun. The laptop doesn't hibernate; only sleeps. I also wish it was bluetooth enabled.

This Laptop requires revisions

POSTED BY: Das Clo , Miami, FL
Overall rating: 3 out of 5 3 out of 5

I bought this M505-S4972 on an impulsive buy, paid too much for it, but i guess its my fault for not looking into the model before buying. There are problems with the air card from what ive read, even though i will never use it. There are some other issues with the machine i cant quite put my finger on, but i know they exist, usually when i see windows animations not working it means something is clashing with something else in the background. Lack of Restore CD/DVD's, had to pay for them to restore the machine, which did not fix anything. Overall i think this laptop is not a great buy, but alas, im stuck with it for now. Would've definitely not have bought it if had known about the little details. Do you have any sort of bios updates or hardware/software updates as of Jan 2010???

Will not connect to AT&T existing service

POSTED BY: Bee , Sacramento
Overall rating: 2 out of 5 2 out of 5

Malfunctioning Fn F8 hotkeys, Error messages on Toshibas WANN Manger. WIll not read AT&T sim card equipped with the computer. WAN light won't stay on. Sleek and beautiful design, nice features, fabulous feel to keypad. Can't use with AT&T Air card/ Broadband.

MSRP: $739.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4300
  • Windows 7 Home Premium (32-bit)
  • 3GB DDR2 800MHz memory
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • 3G Wireless WAN powered by Gobi™ (HSPA/EvDO)
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories