Satellite M645-S4048 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»


POSTED BY: babiie_chiyo , Garden Grove, CA
Overall rating: 5 out of 5 5 out of 5

I just bought this laptop, runs very good. whats best about it, is that it does'nt overheat! LOVE IT! i use it for school and home! i recommend this to college students like me ! perfect size too, not too small, not too big.

Laptop for Delelopers of Software

POSTED BY: jaime85 , Colombia
Overall rating: 5 out of 5 5 out of 5

This laptop is very good, It has a good balance of style and efficiency, the configuration of laptop is ideal for developer of sofware. I recommend this laptop.

Good Laptop for Developer of Software

POSTED BY: jaime85 , Valle, Colombia
Overall rating: 5 out of 5 5 out of 5

This laptop is very good, it has a good balance of style and efficiency. This laptop is ideal for a software developer.

Great Laptop

POSTED BY: Journeyman , Kinnelon, NJ
Overall rating: 5 out of 5 5 out of 5

I traded up from an HP Pavilion and I am very pleased that I selected Toshiba. This laptop is blazing fast and allows me to run multiple applications. I occasionally watch Blu-ray films on the laptop and the picture quality and sound are superb. I am most impressed with this mode's ease of use.

May I have M645-S4048's User Guide Manual PDF?

POSTED BY: Bourne , Palo Alto, CA
Overall rating: 4 out of 5 4 out of 5

I think that will help me a lot! Actually, now, I dont know how to sleep-and-music, I dont know how to switch the Intel HD and Nvidia graphic card. BTW, if I can get an address to download the Toshiba installation file for my laptop, I will appreciate that forever!

Could be a little better

POSTED BY: Stormrider , Brazil, SC
Overall rating: 3 out of 5 3 out of 5

There are three flaws in this notebook that bugs me. The lack of bluetooth and a decent graphic card are two of them. This laptop is definitelly not for gaming, even though there is noneless then a 6.8 Windows score processor here. The third and major flaw is the heat that comes out of the right side of the laptop, so if you prefer to use a mouse instead of the touchpad (like me), the heat is going to be very annoying to the hand. A geforce 310m would be way better than a blu-ray drive. Maybe in the US it`s a value for the money, not my case though. In the good side, the processor is very powerful, I love the LED backlit keyboard, the sound is above average for laptops, can do about 3 hours on battery and...this laptop is VERY stylish and beautiful.

MSRP: $899.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-450M processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • Blu-ray Disc™ ROM (BD-ROM) and DVD SuperMulti drive (+/-R double layer) with Labelflash®

shop for accessories