Satellite P305-S8906

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Suprising Buy

POSTED BY: Mike
Overall rating: 5 out of 5 5 out of 5

Toshiba was the last laptop brand I'd consider buying or even looking at. I was stuck on Dells, HPs and Sonys. A friend recommended taking a look at one. I did, the specs met my requirements- and when combined with the price- exceeded my expectations.

Best Laptop Ever!

POSTED BY: NASA Process Egineer , NASA Virginia
Overall rating: 5 out of 5 5 out of 5

I am a Process Engineer with NASA, and I needed a laptop with this power and reliability. I am extremely pleased with the performance and quality of this laptop. Dr EM

So far so good... give'r a shot.

POSTED BY: John , Texas
Overall rating: 4 out of 5 4 out of 5

I have been using this beast for about 3 days and am pretty happy with it. I am running on a free (hotel) broadband connection that is not that good so I cannot test the full potential of this thing. I am very happy with the sound that comes out of the speakers and the layout of the keyboard is really easy to get used to. I hated typing on my last laptop but this one is very much like a desktop keyboard. I am a little disappointed that it does not have a bluetooth antenna in it but I can plug in a dongle ad take care of that when needed. I have only used the CD ROM one time so I have no opinion on that part. I have not used the wireless but am looking forward to that as well. Wireless (n) will be pretty nice. Display is awesome and should be able to handle any game that I throw at it. I should be able to test it with World of Warcraft tomorrow and I will let you all know.

MSRP: $899.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor T6400
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories