Toshiba Satellite P55-A5200 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great laptop!

POSTED BY: a user , New York
Overall rating: 5 out of 5 5 out of 5

I bought this laptop in July and I absolutely love it! I've had no problems so far. Sound and graphics are great, and it's so much faster than my old laptop. Nice and light with great features. Highly recommended!

BEST EVER!

POSTED BY: marge123
Overall rating: 5 out of 5 5 out of 5

Runs everything great fantastic!

display's angle of view

POSTED BY: dave
Overall rating: 4 out of 5 4 out of 5

Beware buyers! The display's angle of view is very tight/bad. I've got an old ACER laptop (>5 yr old) that has a better display than this new Toshiba. Very disappointed.

Look Around Before You Buy

POSTED BY: Rocky , Ohio
Overall rating: 2 out of 5 2 out of 5

I only had this laptop for around 4 months and the hard drive malfunctioned. I'll give credit to the customer support with directions to send it in, but a fairly pricey laptop should last at least 3 years before something like this happens. Also, you have to pay for the box to ship the laptop even if its under warranty. Before it crashed it did everything that I wanted it to do no problem. Then one day it just quite responding.

Lap too hot on lower right corner

POSTED BY: SoftwDev1 , Guadalajara, Mexico
Overall rating: 2 out of 5 2 out of 5

Good lap, except for this. It's very common to rest hand on right side of touchpad while typing, problem is that this area gets hot and unconfortable, which is obviously an error of design. The fan should be some other place, like on right side of the touchpad, by example.

Toshiba P55-A5200

POSTED BY: traveler , Oregon
Overall rating: 1 out of 5 1 out of 5

We purchased this brand new. In less than 48 hours it crashed. Too bad, had a lot f realy nice featrues. We had to take it back. BUYER BEWARE: With Windows 8, in order to use the apps and email on the computer, you are required to set-up an account, which requires your name, address, email address, dateof birth. HELLO- GOOD-BYE IDENTITY. I do like the Toshiba brand. the performance of this computer was great-til it crashed

MSRP: $754.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories