Toshiba Satellite P55t-A5116 Touchscreen Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: sat5
Overall rating: 5 out of 5 5 out of 5

Great Laptop. Not a fan of Windows 8 because I do not need a Microsoft account except to use most of the features on the home page. I have to use Chrome for work and have everything through google and it isn't as compatible as it could be.

Enjoying this Laptop

POSTED BY: sandrazena , Green Valley, AZ
Overall rating: 5 out of 5 5 out of 5

I was not sure about getting a Touchscreen, but after comparing this Toshiba model with others I opted for it. I like the key board - backlit, nice size, and also very nice touch. I also like the sturdy construction of the laptop itself.

own a few Toshibas....best product to buy!

POSTED BY: mtnbikemadman , Boulder, Colorado
Overall rating: 5 out of 5 5 out of 5

The quality of Toshiba seems to be excellent....I have owned all the major brands, and I now have 3 Toshiba laptops....won't even consider any other brand, other than Apple, when purchasing a laptop! Never once had any hardware issues with any of my Toshiba laptops...quite impressed!

Excellent

POSTED BY: Gentleman john , honeoye falls ny
Overall rating: 5 out of 5 5 out of 5

A perfect laptop for a non-teckie. Easy to use and fun to operate.

Nice laptop and easy to use!

POSTED BY: Rey , Brooklyn, NY
Overall rating: 5 out of 5 5 out of 5

I was very please with my new Satellite Touchscreen! Very easy to use and I was able to load my software seemlessly. Great choice!

Amazing laptop

POSTED BY: Kelly , Danbury ct
Overall rating: 5 out of 5 5 out of 5

It is a very good laptop that's is worth anything

Above my expectation

POSTED BY: Neco , Itapira,SP, Brasil
Overall rating: 5 out of 5 5 out of 5

I'm very pleased with the purchase of my first Toshiba.Nice design excelent keyboard and good performance.

Great, except Windows 8

POSTED BY: Dr O , Charlotte, North Carolina
Overall rating: 5 out of 5 5 out of 5

The machine is great. I love every aspect of it from the keyboard, rapid engagement, back lighting, and overall performance. The problem is Windows 8. IT is cumbersome and frustrating. I would gladly return to Windows 7. The machine is terrific and Windows 8.0 is terrible. ( My rankings are as if the computer had Windows 7.)

Trusted Name in Laptops

POSTED BY: RobC , Pinon Hills, CA
Overall rating: 5 out of 5 5 out of 5

This is the third laptop I have purchased bearing the name "Toshiba". They have all lasted and refuse to die. As a result, I have purchased a new one to stay ahead of technology. The only issue I ever have with Toshiba is that the batteries do not last as long as stated. Having said that, I have also noticed that my new laptop battery does not last that long. Great computer though, I would own nothing else.

excellent computer

POSTED BY: jmw , murfreesboro, TN
Overall rating: 5 out of 5 5 out of 5

You really do get a great computer for the money you spend on it. Touch screen is great and it is very fast. The screen clarity is superb. Would recommend this computer

An impressive laptop

POSTED BY: gandy , n adams, ma
Overall rating: 5 out of 5 5 out of 5

A nice setup. Not cheap but well worth the price. I hate bottom end machines as they just do not perform. The i5 chip is plenty fast enough and Toshiba has made a well balanced laptop here. I've been using and building PC's since the mid 70's so I have a good feel for what works and what does not. This laptop is a very good value for the price and has all the bells and whistles most would want. I am not a gamer so I can not comment. Other than that you will not be disappointed.

POSTED BY: Jersey Shore , Ocean Gate, NJ
Overall rating: 5 out of 5 5 out of 5

The Toshiba is user friendly & the price point is good. This is my second Toshiba. There are some mice improvements. The key back light is a nice feature and the touch screen is simple to master.

POSTED BY: canman , kY
Overall rating: 5 out of 5 5 out of 5

I like the features like LED Keyboard which helps in low light times. I also like the fact that you can deactivate the touch pad when typing.

Fast Laptop

POSTED BY: Cathy , Fond du Lac, Wisconsin
Overall rating: 5 out of 5 5 out of 5

2nd Toshiba laptop. EXCELLENT product!

POSTED BY: Boo
Overall rating: 5 out of 5 5 out of 5

Good Products

POSTED BY: Rick , Crosby, TX
Overall rating: 5 out of 5 5 out of 5

I have owned nothing but TOSHIBA laptops. While others I know have had problems with the other brands, I cannot complain about any of the TOSHIBA's I have owned.

POSTED BY: Doctor Bob , United States, tijeras, nm
Overall rating: 5 out of 5 5 out of 5

entering into this centery

POSTED BY: jerry spinger , carol stream il
Overall rating: 5 out of 5 5 out of 5

I'm 52 yrs. old never worked with a computer so for the last year been looking to enter this century! looked at so many different brands and types they jest did not feel right or comfortable for me the min. I saw and touched this computer I new this was it. jest perfect in every way!! jest magnificent!! so glad I kept shopping would not ben happy with any other computer in the would!!!

POSTED BY: Sammy , Midland, MI
Overall rating: 5 out of 5 5 out of 5

New Laptop

POSTED BY: Syl , Hacienda Heights
Overall rating: 5 out of 5 5 out of 5

Excellent

POSTED BY: Cookiec52 , Coulterville, IL
Overall rating: 5 out of 5 5 out of 5

I bought this laptop to use in my Sewing room to put my embroidery designs on and make them more accessible. It is just what I wanted and performs nicely.

My first touch screen

POSTED BY: New to electronics , Bishop, CA
Overall rating: 5 out of 5 5 out of 5

Great performance and value

POSTED BY: sammy , emeryville CA
Overall rating: 5 out of 5 5 out of 5

All the features I wanted for the lowest price around. Speed, user friendly, perfect!

excellent choice!

POSTED BY: HLG , Niagara Falls, NY
Overall rating: 5 out of 5 5 out of 5

After hands on testing of multiple computers at several different vendors, I kept coming back to this Laptop as it had all the features that I wanted, no compromise. It has proved to be a top notch performance laptop!

learning curve

POSTED BY: rmc51534 , glenwood ia
Overall rating: 5 out of 5 5 out of 5

has windows 8 learn how to all over again

Great value!

POSTED BY: EJ , Round Lake, IL
Overall rating: 5 out of 5 5 out of 5

It took me a while to get used to WIN 8.1, but I love my P55t laptop. It boots quickly, connects to my network with no problems and does work and play very well. The 15.6" screen is beautiful and a great compromise between 14" and 17". I mostly use it as a desk-based system, but could use it on the go as well. So far it's taken everything I thrown at it very well, i.e. office items like documents, spread sheets and presentations as well as web surfing and movie watching. I'm pleased with my purchase.

Premo Laptop

POSTED BY: LeoH , East USA
Overall rating: 4 out of 5 4 out of 5

Nice features backlighted keyboard, and great specs. Just set up my brothers new laptop, the Windows 8 takes a little getting use to, and a USB mouse may be considered, as touch pad clickers are a little hard to use, a printed manual would be nice to include, as access to features on set up is not easy.

Windows 8.1 PC Review

POSTED BY: RW , Phoenix Az
Overall rating: 4 out of 5 4 out of 5

This is the first Toshiba PC I have had in about 25 years. I respect the brand and believe they make quality products. I have not had any issues with the computer but do not care for Windows 8.1 and the touch screen causes me to do things I don't want to do/happen. I don't find the new windows intuitive and have a hard time getting back to basic computer file activities.

Touch is fun

POSTED BY: BJ , Durand, WI
Overall rating: 4 out of 5 4 out of 5

So far this laptop has worked extremely well. The touch screen works good too. The software has become very complicated but Toshiba help has been very useful and the User Guide clears up many questions I have. I have some computer background and I feel sorry for those older folks trying to get things set up properly. This is my 4th Toshiba laptop and I will always be a fan for the machines are tough and run well.

Very Reliable Laptop

POSTED BY: Georgia , United States
Overall rating: 4 out of 5 4 out of 5

Only con is the battery life. I handle that by keeping my cord nearby

Laptop Luxury

POSTED BY: Grammy7 , Cheswick, PA
Overall rating: 4 out of 5 4 out of 5

After 10 years with a desk top, the laptop seems like a luxury item! With wireless, I can take it anywhere in the house or patio. Great for use!

Nice except fo Windows 8/8.1

POSTED BY: Thinkfast , San Francisco, CA
Overall rating: 4 out of 5 4 out of 5

This laptop has many features for a Windows 8 computer. The problem is its a Windows 8 computer! It has a full HD touch screen to take advantage of Win 8.1 features. I would prefer a faster processor, but it is adequate for most users. The keyboard is nice with adequate spacing. The overall look is nice and clean. If I were to improve this computer I would install Windows 7 (most important) and possibly upgrade the processor. Memory is good as is the hard drive capacity. 90 days of tech support is much less than the competition, which is why I would not have to be selective on which friends I might recommend Toshiba. But, I would recommend this laptop for tech savy users who know if this machine is good for them.

Great Quality Laptop!

POSTED BY: TechLover1992 , Dora, AL
Overall rating: 4 out of 5 4 out of 5

After owning a Toshiba that was Windows 7 and ran on an i3 Intel Core processor, I found myself getting highly frustrated with the performance of the laptop compared to how much I used it so I decided to research laptops and find something more suited to my needs. After reviewing many (Toshiba) laptops, I found this one had the best rating and quality for the price range, operating system, and processor. I LOVE this laptop and all the features it comes with including TouchScreen, Apps, overall speed, and graphics. This laptop handles my multi-tasking and usage without a hitch. I do a lot of research, watch many videos (including many on iTunes), and spend a good bit of the day on the laptop. Great battery life and quality laptop!

tryingmybest

POSTED BY: Starter
Overall rating: 4 out of 5 4 out of 5

Stylish performer

POSTED BY: mrhoff , abilene, tx
Overall rating: 4 out of 5 4 out of 5

have used for about two months now, impressed with how light this unit is as compared to past units I have owned, lighted keyboard makes operation anytime a plus

Great laptop so far.

POSTED BY: Kim , Florida
Overall rating: 4 out of 5 4 out of 5

Love the laptop but hate the mouse location. It is to far to the left (centered to the alpha keys). Great picture quality. Videos run with no lag time. Purchased because I still want a DVD slot and most no longer offer. Love it so far. Window 8 is hard to get use to but the touch feature on this computer works great too.

Good with reservations

POSTED BY: AF , Hayward, CA
Overall rating: 4 out of 5 4 out of 5

I've had several iterations of Toshiba laptops and always liked them a lot. I like this one a little more in some areas, a little less in others. To be fair, some of it isn't the fault of Toshiba, some is the frustration of Win 8/8.1. I especially like the full keyboard with number keypad. The display is beautiful! I also like that it connects easily with a bluetooth keyboard. I was a little frustrated with the screen locking up and/or going to black screen or just getting stuck in an endless loop of "please wait" - especially since I couldn't just pull the battery as in my previous versions (the battery in this one is internal). However, now that I've found the battery re-set, that frustration is a little dampened; however, the (many) causes to have to re-set are extremely frustrating. Would I buy another Toshiba? I'd probably give it one more try, but since this is a new computer, I hope I won't have to consider it for a while.

Great laptop

POSTED BY: AMS , Rancho Cordova, CA
Overall rating: 4 out of 5 4 out of 5

I originally bought the first laptop for my daughter's birthday gift. After I started setting the laptop all the different apps and versatility made me realize that I need it to change my own laptop that I have own since 2006, the difference in speed and graphics was spectacular. So I purchased one for my self and I am very satisfied with it.

Good Laptop-Bad Windows 8.1

POSTED BY: Coldwarrior , Sterling Heights Michigan
Overall rating: 4 out of 5 4 out of 5

The hardware on this is excellent, Good design. What is irritating is it is impossible to remove Apps that I will never use ie: Games. But there are others. I don't know if Toshiba or Microsoft is responsible for the useless apps but there should be a way to delete anything unwanted. There should be a Power Off Screen button. Cursuring to the bottom right is tedious and sometimes takes several attempts. Normally, I use the windows/C or D to do it.

Desktop Replacement

POSTED BY: SeaDragon , Tampa, FL
Overall rating: 4 out of 5 4 out of 5

I bought this laptop as a desktop replacement and so far I have not been disappointed. The final selection criteria came down to the fact that it had an optical drive and very good speakers. I have liked the keyboard lighting feature and the offset numeric keypad.

Windows * is the PITS

POSTED BY: Bob , Whittier, NC
Overall rating: 4 out of 5 4 out of 5

Good Computer, Hate the Windows 8

Great Laptop

POSTED BY: Jan , Grand Prairie, TX
Overall rating: 4 out of 5 4 out of 5

I absolutely LOVE the laptop...but I hate Win8. I realize that isn't your fault, but it is worse than Vista. This laptop with XP would have made me VERY HAPPY.

New To Toshiba brand laptop

POSTED BY: Miggy , Trenton MI
Overall rating: 4 out of 5 4 out of 5

After getting tired of HP and the poor quality of their product as well as terrible tech support I decided to try Toshiba. So far I haven't had any problems with my new Toshiba Laptop. It's fast and has all the features I need. My only concern will be down the line when the battery starts to go bad. I hope it will be easy to replace since it appears I will have to open the Laptop case itself.

Improv app performance

POSTED BY: Thom , Marion, IN
Overall rating: 4 out of 5 4 out of 5

Many apps I have worked with will crash unexpectedly and frequently. It is not a problem with the apps themselves, but with the computer's ability to run them

Good Laptop...How To Instructions -- missing

POSTED BY: columbia , Columbia MO
Overall rating: 3 out of 5 3 out of 5

I like the laptop--touch, feel, size, but still (after two months or more) still figuring the most basic things out.

good laptop, great computer

POSTED BY: sugarfoot , Sugar Hill GA
Overall rating: 3 out of 5 3 out of 5

Probably the best and certainly the most powerful laptop I have ever owned. Not happy with the level of bloatware. I have spent hours trying to get rid of software I will never use.

mouse pad quit one month after buying

POSTED BY: jake , iowa
Overall rating: 3 out of 5 3 out of 5

I like this laptop a lot I actually was loving it then one day I opened it and the mouse pad off indicator light was on and the pad wouldn't work. I pressed the FN+F5 key to turn it on and it won't work. Now its not unusable because its touch screen but it gets annoying having to use that all the time.

New Toshiba Satellite

POSTED BY: Beckers , Tampa
Overall rating: 3 out of 5 3 out of 5

I was so excited to get a new computer and I had a Toshiba that had finally bit the dust and I had been happy with it- so I went with Toshiba again. I have been so disappointed. Even with Intel 5 it is the slowest computer I have had in a long time. The flattened screen is also a bit difficult to get used to. When I got my "NEW" computer home I found books already downloaded on it. I found about 15 multimedia items already loaded on it. getting used to windows 8.1 is a challenge but doing it with a frustrating laptop makes it more difficult.

POSTED BY: Swampy , Minnesota
Overall rating: 3 out of 5 3 out of 5

My Keyboard stopped functioning after only 28 days. I returned it and accepted another of the same model. I was not Happy.

Great feature set, avg speed

POSTED BY: tduemig , Margate, FL
Overall rating: 3 out of 5 3 out of 5

Loved the styling and feel, but the speed is lacking. The i5 4200u is a fast enough processor but using 5400rpm spindle hdd is counterproductive. The screen also took a ton of tweaking to "look" right but once configured that was a non-issue. As a programmer I need beter performance so I returned this unit.. it also didnt make sense to upgrade to the i7 4500u machine as its not a true quad core. However the major selling point for me was the DTS sound.. best sound on any laptop I looked at... so much that I ordered a s55t with i7 4700mq processor instead.

Buyer Beware!

POSTED BY: Will , scranton,PA
Overall rating: 2 out of 5 2 out of 5

Problems with touch capability. On computer #2.

New laptop faulty

POSTED BY: Paul , Southwest Idaho
Overall rating: 2 out of 5 2 out of 5

Bought a brand new laptop and after less than 2 weeks of light use the hard drive failed.

Started Out Bad

POSTED BY: PEA , Austin, Texas
Overall rating: 2 out of 5 2 out of 5

Never keep a good connection to the internet. However since I first purchased this laptop Toshiba has released a new driver that was installed and now I love this computer!

poor wifi connection

POSTED BY: saunder , TX
Overall rating: 2 out of 5 2 out of 5

Since I bought it home, I found at least 50% of time it cannot be connected to the WIFI, or the connection will be broken abruptly. However, the other computers, IPADs, or I-Phones in my home have no problem at all. I even wanted to return it 3 weeks after purchasing it. Depressed.

Really hard to use

POSTED BY: Ana , NY, NY
Overall rating: 2 out of 5 2 out of 5

There are a coupe of things i really don't like about the laptop - the most disturbuing is that the right click is so narrow that it's basically nerve wracking to use. And I use it a lot. Every time I touch it, because it's that narrow, I also touch the the main touchpad area and the laptop reacts as if it was a normal click. Sometimes, even if I only touch that tiny little area, I still need to press a couple of times until it reacts. It is beyond annoying. I've been using laptops for over 15 years, and I know how to use a laptop. My fingers are fairly thin also, that could not be the reason of this problem. - it is very heavy - it has some adds on it that are popping up as some small videos that I didn't figure how to get rid of - it has a narrow, long screen. Because most of the websites are still built on square screens I have to carry this humongous laptop but I only see images on a tiny little area in the middle of my screen.

Worst product ever

POSTED BY: George , NY
Overall rating: 1 out of 5 1 out of 5

First laptop lasted three weeks. Replacement lasted 45 minutes.

Not at all Useful

POSTED BY: PeerGynt , Bellingham, WA
Overall rating: 1 out of 5 1 out of 5

Looks nice, but is unable to stream info, trailers, films, etc. Can't even watch a 2 minute movie trailer without it stopping 4 or 5 times for data stream to load. It just sits on my desk. If I need to download anything, I have to do it on my 5 year ols HP computer, transfer data on a zip drive to my brand new Toshiba. What a waste!

Not Good

POSTED BY: hocrya , MN
Overall rating: 1 out of 5 1 out of 5

Operating system loaded up with viruses right away. I had to reload windows. It cost me lots of extra time and money to get it working properly.

Don't buy

POSTED BY: VWM , Queens, NY
Overall rating: 1 out of 5 1 out of 5

When plugged in it has an electric field on all metal surfaces. Geek guys couldn't feel it. Customers could. They replaced the AC adapter. I had already done that. It still has the problem. Sometimes it is faint and sometimes it is quite strong causing a stinging to my wrists when typing. I also replaced Windows 8 with Windows 7. Geeks said, "We have never heard of this problem before." Read other reviews. I'm not the only one complaining.

Keyboard malfunctions

POSTED BY: Labor Lawyer , Little Rock
Overall rating: 1 out of 5 1 out of 5

One diagonal row of keys -- 8, i, k, comma, and the down arrow -- periodically stops responding on the keyboard and I have to switch to the on-screen keys. This slows down my typing and obscures half my document! I am a lawyer and bought this machine for word processing. Big mistake.

POSTED BY: steve , flushing ny
Overall rating: 1 out of 5 1 out of 5

less then month old need repair on harddrive

MSRP: $895.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-4200U Processor
  • Windows 8.1
  • 8GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories