Toshiba Satellite P75-A7100 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Deal Great Product

POSTED BY: Drew , Burleson, TX
Overall rating: 5 out of 5 5 out of 5

This thing is definitely worth the great value. Most of the other laptops in its class were all touch screen, something that I'm not particularly fond of or in need of. So to get this computer with the specs that it has at the value that it's being offered is a HUGE plus for me. The processor is quick, has a ton of memory. It's smooth and fast. Definitely enjoying it so far!

i7 Laptop

POSTED BY: Pinklacedd , Cheyenne Wy
Overall rating: 5 out of 5 5 out of 5

Love my laptop. I have stuck with toshiba and only had a screen problem on my fist one. The are durable and are easy to use

Up there with the best.

POSTED BY: Satellite user , Rochester Hills, Michigan
Overall rating: 5 out of 5 5 out of 5

Good looking and performing laptop.

GREAT LAPTOP! AWESOME FEATURES!

POSTED BY: ilconsigliere , MIAMI, FLORIDA
Overall rating: 5 out of 5 5 out of 5

Great laptop! Highly recommended! Can't find any cons. Maybe Windows 8.1, but that's Windows, not Toshiba. Super-fast with Intel Core 7. Fantastic features like the backlit keyboard. No flaws whatsoever.

Good decision

POSTED BY: DC , Pennsylvania
Overall rating: 5 out of 5 5 out of 5

Very pleased with my laptop selection. Little pricey.

WOW

POSTED BY: Gladiola , Springvlae ME
Overall rating: 5 out of 5 5 out of 5

other then going from windows xp to 8.1 takes a lot to get used to, but all in all a very good computer for what i use it for.

My first laptop

POSTED BY: Cactus Flower , La Quinta, CA
Overall rating: 5 out of 5 5 out of 5

I am getting used to a new keyboard, touch mouse, etc. It is not as difficult as I thought. However, I have resulted to using my old mouse, and pad.

Love it

POSTED BY: New to Laptops , Beaufort,SC
Overall rating: 5 out of 5 5 out of 5

Very fast,sharp video screen, great sound. This is replacing my old desk top PC. So far no problems.

Its good

POSTED BY: Chet , Bloomington Il
Overall rating: 5 out of 5 5 out of 5

It has everything I need the screen size the backlit keyboard I am enjoying it very much it has all the speed I need

Very nice

POSTED BY: Hankster , Singer Island FL
Overall rating: 5 out of 5 5 out of 5

Well this is my fourth Toshiba and I am very happy. The nice surprise was that when I opened the bottom to add more memory I discovered a section tonadd a second hard drive. Purchased another 1T hard drive, set up the bios and it worked fine. Nice surprise.

excellent for me

POSTED BY: VIC-JAMES , CHICAGO,ILL.
Overall rating: 5 out of 5 5 out of 5

perfect for djing and storing multiple music programs!!!

Truly an excellent laptop

POSTED BY: JPK , Boone, NC
Overall rating: 5 out of 5 5 out of 5

The laptop is a good value for the money. I personally like the Intel i7 2.4 that boosts to 3.4 according to the number of tasks that you have going. It comes with 8 GBs of memory and 750 GB hard drive. I also like the built-in burner/player. I may purchase Toshiba's 128 GB SSD and put it in myself to give it a little more punch. Finally, the 17.3 Full HD screen is absolutely gorgeous with a beautiful brushed aluminum finish inside and out. This is the best laptop I have ever had and the key pad lights up too.

Outstanding value for price, all the features

POSTED BY: Hub , Hubbardston, MA
Overall rating: 5 out of 5 5 out of 5

Great Laptop

POSTED BY: Gramma , Great Falls, MT
Overall rating: 5 out of 5 5 out of 5

I love my computer. Wish the battery lasted longer. It took me a while to get use to the new features. Still getting there.

Absolutely Awesome

POSTED BY: NanaSharon , Birmingham, AL
Overall rating: 5 out of 5 5 out of 5

We had a house fire on April 11, and unfortunately my computer was water damaged, so I had to get a new one. I vowed, "No more HP's!" I'm glad...I'm loving this one!

Great laptop for light gaming and movie watching

POSTED BY: Dusty
Overall rating: 5 out of 5 5 out of 5

This laptop is great for watching movies and playing games like star craft 2. It has an excellent display and great sound. One of the best perks is the ability to upgrade the ram and put a second hard drive in if you really want to boost performance. It is great for my needs as is but still nice to have the options. Would also make a great laptop for college work. Wish I had this one in law school.

Indeed the best laptop ever!!

POSTED BY: Angel , Huntsville, AL
Overall rating: 5 out of 5 5 out of 5

Such speed (getting to site to site) such quality such ease( being able to understand with precise steps to get the job done) with vision problems the lighting up when touch is phenomonial I can go on and on just amazing! Thanks, Angel

great bang for the buck

POSTED BY: phqic , mich
Overall rating: 5 out of 5 5 out of 5

i7 fast plenty of memory and good looks. mostly good set up

Great laptop

POSTED BY: Bwillow , Mt Vernon, TX
Overall rating: 5 out of 5 5 out of 5

This was an excellent value. Easy to use, super fast. I like the screen as well. Great sound. This is the 4th Toshiba laptop I've purchased and they are great.

Loving my new laptop!!

POSTED BY: Hzleyes48 , Oxnard, CA
Overall rating: 5 out of 5 5 out of 5

The backlit keys are awesome. They make using the laptop easier in low light. I like the feeling of the keys. We have only had Toshiba laptops and wouldn't have any other brand.

Best laptop of many

POSTED BY: Chupacabra , Milford, OH
Overall rating: 5 out of 5 5 out of 5

Faster than light

POSTED BY: IsoSpear , Chicago IL
Overall rating: 5 out of 5 5 out of 5

My new Toshiba laptop is amazing! It has the newest Intel driver i7 so it runs very well and very fast. I love it.

POSTED BY: tom , Naperville, IL
Overall rating: 5 out of 5 5 out of 5

good Laptop

POSTED BY: cornfetti , Stuart, FL
Overall rating: 5 out of 5 5 out of 5

great

POSTED BY: cab , midland,mi
Overall rating: 5 out of 5 5 out of 5

Excellent Laptop For Graduate School!

POSTED BY: Antwonne , Earth
Overall rating: 5 out of 5 5 out of 5

I have previously owned other name-brand laptop PCs before; however, I must admit that this Toshiba Satellite P75-A100 is far and above the best of them all. I am most sincerely impressed by the very high quality of construction, and also the many Toshiba apps that make owning this new PC a pure joy! Keep up the excellent work!!!

Excellent Laptop

POSTED BY: Tarheel , Riverview, Fl
Overall rating: 5 out of 5 5 out of 5

So far it performs well. Still getting use to it but it is easy to use and very fast. I love the metal case.

great laptop

POSTED BY: mo , nj
Overall rating: 5 out of 5 5 out of 5

worth the price. i use it mostly as a desk top.

Excellent laptop, but hard drive/fan noisy

POSTED BY: Cindy , Southfield, MI
Overall rating: 5 out of 5 5 out of 5

The laptop is excellent, but the hard drive/fan is very noisy at startup plus a few minutes.

POSTED BY: DubyaB
Overall rating: 5 out of 5 5 out of 5

Serious Leading Performer

POSTED BY: RDH , Alexandria, VA
Overall rating: 5 out of 5 5 out of 5

Great hard disk performance, nice software/feature set, great audio playback, good USB tight sockets improvement over former competitor, good enough to compete with desktop performancewise.

Great Laptop

POSTED BY: DJDrew , Panama City Florida
Overall rating: 5 out of 5 5 out of 5

after my last laptop broke do to me dropping it I went searching for something premium, I have had Toshiba in the past and always have had great luck with Toshiba products. I found this one which has everything I need regarding speed and power to run my music work. the screen size, HD quality, Harmon/Kardon sound, and the super I7 processor to support it all makes this laptop great I am very happy. the only thing I could ask for more would be a longer battery.

computr 4

POSTED BY: patsy , sargent tx
Overall rating: 4 out of 5 4 out of 5

This computer goes to spanish every once in awhile and my son-in-law has to come put it back to english. I speak o spanish! So I live where there are lots of Mexican people why was it set up this way ehy? But it\/s been just fine just bilingual and that does not fly with me.

My New Laptop

POSTED BY: Not a Geek , Broomfield CO
Overall rating: 4 out of 5 4 out of 5

The P75-A7100 laptop that I purchsed a couple days is as always well made and with no problems. I have been purchasing your products for many years now and look forward to this laptop lasting at least as long as all my previous models.

Great laptop

POSTED BY: rickhr , Raleigh, NC
Overall rating: 4 out of 5 4 out of 5

Great laptop but significant problems with Microsoft Windows and Office 2013. Microsoft spent 2 hrs on the my laptop and could not fix.

very nice laptop

POSTED BY: Nickie , Midland, Tx
Overall rating: 4 out of 5 4 out of 5

This laptop looks good and it has all of the features I was looking for. I am pleased with everything about it. HOWEVER, it needs to come with a Toshiba brand Flash-drive to do the initial recovery because it will not accept any other brand.

Nice laptop

POSTED BY: Ethel , Western NY
Overall rating: 4 out of 5 4 out of 5

has a few things it doesn't need-like the button to disable mousepad!!!! I finally found it and turned the pad on again. If it is as reliable as the old one it will be a good purchase. Still getting used to windows 8.1 which is a hair better than 8.

8 second boot time

POSTED BY: Smackwater Jack , Lakewood Ca.
Overall rating: 4 out of 5 4 out of 5

I added an 128 gig SSD drive, and 8 more gigs of RAM (Very easy to do btw) Put the OS on the SSD and everything else on the orig. HDD and this thing screeeeeeaaaaams. Lovin' it so far. Thanks Toshi!

Good product

POSTED BY: B
Overall rating: 4 out of 5 4 out of 5

My favorite feature is the lighted keyboard - the looks, smoothness and feel. My least favorite are the USB and SD card slots, they seem to have a rough edge and neither the USB cord nor my camera card go in easily. The button that opens the DVD drawer is hard to feel. I have to lift the laptop on its edge to find it. I still don't like the Windows 8.1 installed on it - the illusive "charms" , there's no simple easy to find, Start, all programs or control panel like on Win. 7. Performance wise it seems o.k. Battery life seems about 3 hours.

POSTED BY: gas , Ohio
Overall rating: 4 out of 5 4 out of 5

The only complaint I have is no scroll wheel.

Very Good laptop

POSTED BY: Tobey , New Town, ND
Overall rating: 4 out of 5 4 out of 5

This is a very user friendly laptop that I would highly recommend.... Easy setup!

Good laptop

POSTED BY: gregsmom , Strafford, PA
Overall rating: 4 out of 5 4 out of 5

Most laptops are so small that I'm not comfortable using them. This one is a good size, and so far, the performance has been good.

Toshiba Intel Quad to replace HP Quad

POSTED BY: PatrickC7 , Mission Viejo, CA
Overall rating: 4 out of 5 4 out of 5

This P75-A7100 17" Laptop is quick, energetic, and very easy to use. The ways and operations of Toshiba Support take some learning, but overall All Drivers and Manuals can be obtained easily online. My Particular Laptop did not have a separate Video Ram option but the machine was very responsive with the 8GB min that comes with the system. I added another 8GB from Toshiba - A person ordering Accessories such as RAM needs to make sure you order using their coupons - and the system exhibits of more stability and responsiveness. Toshiba makes a high quality Laptop. I have used HP until recently. Toshiba was able to provide a Laptop that works well for a reasonable price.

great package & full of goddies

POSTED BY: dadof3 , Hickory, NC
Overall rating: 4 out of 5 4 out of 5

I have used several laptops from other companies in the past. I owned a Toshiba before and it performed well. I didn't like the idea of Windows 8 due to using the original version. I do like the changes made to the 8.1. Now, to the laptop itself. I love the big screen and the chicklet keyboard. That is one thing that I prefer over the flat keys that seem to be used on the majority of other laptops. It performs multiple functions quickly and starts up and shuts down super fast. I wanted a laptop that had a DVD player and most have removed that feature for lower profiles. It plays DVD's well and is not easily opened accidentally. Like other computers, it comes loaded with some bloat, but not bad. It has many useful apps included. The only thing that I consider an issue (with all Toshiba laptops) is the power plug. It sticks out like a bullseye just waiting to be hit by something. Over time, that causes it to become loose and not make a good connection. If the plug came out and was angled, that would make it less prone to this issue. Overall, a really good laptop in all categories and I am well pleased.

Love it so far.

POSTED BY: simpleman171969
Overall rating: 4 out of 5 4 out of 5

One of the better laptops when it comes to what you get for your money. Very nice keyboard feel and almost perfect lighting on the keyboard. Just wished laptop manufacturers would start putting more of a rubbery friction surface on the bottom so when you are running a chill pad under the laptop and it is actually on your lap it would not keep sliding around. I super glued felt pads on my last chill pad and it helped but I ended up super gluing them to my old laptop also and so I had one unit and it worked great. BUT I do not want to start super gluing stuff to my new Toshiba! Overall happy so far.

Almost Perfect

POSTED BY: WildBill , Janesville, WI
Overall rating: 4 out of 5 4 out of 5

This is a great laptop. It has good performance and value. If it had a Blu-ray drive and a discreet video chip it would be perfect.

Overall good

POSTED BY: Spike , Boyertown, PA
Overall rating: 4 out of 5 4 out of 5

One draw back is the sound it is very weak and is not good if you want to play movies or play music

Still evaluating, but very nice.

POSTED BY: Jay , Indianapolis, IN
Overall rating: 4 out of 5 4 out of 5

Great graphics, great speed, loads of info at my fingertips. Executes programs well.

Toshiba P75 Laptop Review

POSTED BY: Trader , Upstate NY
Overall rating: 4 out of 5 4 out of 5

New Toshiba is my second Toshiba. I am very demanding about performance. Works very well. Still a mystery to me why batteries are not able to function for 24 hours or more without recharge - something amiss with that technology. Battery life is something that a user should never have to think about.

great price value

POSTED BY: toby , las vegas nv
Overall rating: 4 out of 5 4 out of 5

I basically want a laptop that is a desktop replacement and this computer is perfect for that

Well Built

POSTED BY: Cootus , Battle Creek Mi
Overall rating: 4 out of 5 4 out of 5

Its a Good well built laptop; Dislike the bloat ware, Windows 8.1 still has Issues, SOS,

Toshiba laptop

POSTED BY: master , marshfield, wi
Overall rating: 4 out of 5 4 out of 5

I got the one with the largest screen. Man it is great. For my old eyes is a great thing.would like a little more paper to learn with. Easy to follow makes it nice.

Different than HP laptops

POSTED BY: Doctercoffee , Romulus, Mi
Overall rating: 4 out of 5 4 out of 5

I have to get used to the Toshiba brand, I have used HP laptops for the last ten years. So far so good, I love the backlit keyboard and the s.s. finish of the case.

Great Laptop!

POSTED BY: Gutsy , New Jersey
Overall rating: 4 out of 5 4 out of 5

I love my Toshiba P75-A7100 laptop. I especially like the backlit keyboard. The hinges for the Toshiba monitor are also solid and sturdy compared to my 5 year old laptop .. which broke on me a year or so after I purchased it. I'm getting about 2.5 hours of battery life not 3+ as advertised. Other than that, it's the best I've ever owned.

Function Keys are Weirdly Inverted

POSTED BY: Arbo , Livingston
Overall rating: 4 out of 5 4 out of 5

The machine is blindingly fast, but I have problems trying to use the function keys. On other computers, the keys are defaulted to F2, F3, F4, F5....etc. On this device you must hit the FN key simultaneously to get the Function feature active. One other things, I have a tile floor, and whenever I touch the stainless keyboard with my bare feet on the floor, I feel the slight tingle of electric potential. It is very slight, almost not noticeable.

Laptop

POSTED BY: pinky2 , Yuma, AZ
Overall rating: 3 out of 5 3 out of 5

It is very hard to get rid of apps you do not want, it is also difficult to move apps you do want to the windows page without it opening up every time you touch it. I find the mouse or touch pad gets a little slow at time and you have to left click to get it to move. Windows 8.1 is terrible.

Not yet impressed

POSTED BY: newbie , Durham,NC
Overall rating: 3 out of 5 3 out of 5

Another laptop

POSTED BY: Olduser , Fort Lauderdale, FL
Overall rating: 3 out of 5 3 out of 5

The laptop works fine, but all Toshiba content about games and other apps are just trash for a working computer. Windows 8 not friendly at all.

First new computer in 10 years!

POSTED BY: Ma & Pa , Hugo, MN
Overall rating: 3 out of 5 3 out of 5

This is the first computer in 10 years and our first laptop. It is SO different than our old computer it is taking us time to get used to it. There are game CD's that worked on our old computer that do not work on this computer and we miss them. We have a CD game we purchased 2 years ago that did not work on our old computer because the video on the old was too small, and it is not working on this computer either! I have a family tree that I created on the old computer that this computer cannot read. The tree is 150 pages long so if the Geek Squad cannot find a way to help this computer read it, I will have to spend weeks redoing this tree! Also, I was hoping to share the tree with other family by sending them CD's but will their computer be able to read my CD? Thankfully I have a printed version to work off of to recreate this tree if I need to. I do not understand why things I did on the old will not work on the new when both were run by a Microsoft windows product and both have Microsoft writing programs. With the troubles we have had with our screen freezing and no way to close the game we were playing at the time, we have been forced to do a hard shut down 4 times now and this computer is only one month old! It won't last 10 years like our old one did at this rate. Why don't things get build to last anymore? Overall, I guess this laptop is average for todays products.

New Toshiba laptop review

POSTED BY: Teach , Plattsburgh, NY
Overall rating: 3 out of 5 3 out of 5

I thought that since it had the fastest processor in it that it would process faster. It does not. Additionally, it seems to be always running and hot.

good

POSTED BY: pinhojonas , milford,ct
Overall rating: 3 out of 5 3 out of 5

good

OK laptop

POSTED BY: zeke , Lake Ridge,VA
Overall rating: 3 out of 5 3 out of 5

Keypad is too sensitive. Went into the Toshiba guide and it listed "too sensitive" as a problem, but did not say how to change it.

Good until it crashed

POSTED BY: JQ , Oklahoma City, OK
Overall rating: 2 out of 5 2 out of 5

Overall I like the brand and really liked some of the features this model had but I have not had good luck with the product. Had this model less than one month before it crashed and I took it back to store

Not Good

POSTED BY: Nana , Appomattox Va
Overall rating: 2 out of 5 2 out of 5

Not happy with the battery life and unit gets to hot while using. Battery last 30-45 minuets after charging.

worst experience ever

POSTED BY: mary , east islip, ny
Overall rating: 1 out of 5 1 out of 5

I have had to take this computer back to the store I turn computer off at night and in the morning will not start.

Worst laptop I ever had

POSTED BY: Beaver , Twin Lake, Michigan
Overall rating: 1 out of 5 1 out of 5

This laptop comes with a lot of extra baggage, Norton utilities come on guys Norton is a piece of trash uses way too much memory. Besides Norton utilities there's all kinds of trash software is hard to erase from this unit. I bought this because I need a unit that was reliable so far this unit is about as reliable as walking through a mine field blind folded.

NOT THE BEST LAPTOP, TOSHIBA HAS MADE MUCH BETTER.

POSTED BY: FDR , Toms River, NJ
Overall rating: 1 out of 5 1 out of 5

Not my 1st Toshiba, but may be my last. Most all the keys on the keyboard do not register when typing. The page zooms, plus or minus at will, and sometimes jumps to 10% zoom without touching the keyboard at all. The spacebar does not register unless it's tapped a few times. That also applies to other letters & keys. IE: bB, zZ, wW and a few more. Sometimes while typing, previous sentences are erased. Control Z intermittently may work to restore, same. The curser has a mind of it's own. When gliding across a page, it may suddenly stop, get stuck & 2 to 4 minutes start working again. The bandwidth for videos gets stuck forever, when you try to fast forward or use playback. The e-mails often stick & a new browser window is needed to start again & go forward, especially in drafts. Upon opening a web-site, turning pages is difficult, after page 2, often you cannot proceed any further and the cap lock does not always work correctly, thus upper case not lower, lower instead of upper! The machine is so new, I have not tried all the other features. What happened to Toshiba?

POSTED BY: RK , huntington beach, ca
Overall rating: 1 out of 5 1 out of 5

pain in the neck

POSTED BY: Upnorthbob , Traverse City, MI
Overall rating: 1 out of 5 1 out of 5

hard to use. inconvenient.

MSRP: $948.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8.1
  • 8GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories