Satellite R845-S80 Laptop

Average Customer Rating:

top selling items
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Rockin' Battery Life!!

POSTED BY: tamtam
Overall rating: 5 out of 5 5 out of 5

The battery life on this thing is absolutely amazing. Almost TOO amazing. Also the face recognition is awesome!!

laptop review

POSTED BY: Cupertino mom
Overall rating: 5 out of 5 5 out of 5

For all of the above "star'd" reasons.

I love nothing more that a great TOSHIBA!

POSTED BY: Starkindler , Nutley, NJ
Overall rating: 5 out of 5 5 out of 5

This is my 2nd Toshiba laptop, the first one - a Toshiba TECRA lasted almost 8 years until it became a dinosaur and a thumb drive was invented that had more memory than that entire laptop. Time came to buy a new machine and the Toshiba was my first choice, the price was right, the features were perfect and since I do a lot of digital scrapbooking the screen, weight and size fit best into my lifestyle of travel and working remotely. Great battery!

first laptop

POSTED BY: auntie , wallingford,ct
Overall rating: 5 out of 5 5 out of 5

Very versatile

Love it.

POSTED BY: walty , tampa
Overall rating: 5 out of 5 5 out of 5

Great bang for the buck. Much better than my HP laptop. Fast processor, light weight and long lasting battery. What I don't like is the mouse pad is too sensitive. You have to shut off the mouse pad to type correctly. Its not a Mac, but its a great deal for the money. I would buy another one.

Love it

POSTED BY: Cingetor , Decatur AL
Overall rating: 5 out of 5 5 out of 5

I am using Toshiba product for 7+ yrs and love it!

new to me

POSTED BY: Gary , Dover DE
Overall rating: 4 out of 5 4 out of 5

I am satisfied with its function but have not used it too much yet.

POSTED BY: Neil
Overall rating: 4 out of 5 4 out of 5

The battery is amazing but the speakers are sub-cell phone quality and other extra features are lacking. Very thin and very light. The mouse pad is random at times and not as responsive as other satellite laptops.

Typing errors

POSTED BY: lala , Los Angeles, Ca.
Overall rating: 4 out of 5 4 out of 5

There is a problem with typing. While i type it can suddenly jump a row or a line and continue typing elsewear. If I don;t look at my typing for a few seconds it can mess up my whole page. I don't know why it happens. Make sure it doesn't happened in your computer if you by a Toshiba

Uncontrollable cursor

POSTED BY: teachergal
Overall rating: 4 out of 5 4 out of 5

Paid too much to have an erratic cursor. I type a lot and I need the cursor to stay on the line I am typing not jump somewhere else. Battery-life is excellent though and is my favorite feature.

slow

POSTED BY: chicky , india
Overall rating: 4 out of 5 4 out of 5

At starting stage it will be very slow when we start up thelape

great laptop

POSTED BY: AJ , Boston, MA
Overall rating: 4 out of 5 4 out of 5

This is my first laptop, so I cannot compare this with other laptops, and I cannot tell if some of the problems I encounter have more to do with being a laptop neophyte or if other laptops would present fewer challenges. Primarily, the keyboard and FN keys seem to be ultra sensitive. As a person who is very fast on a keyboard, I kept having problems with the curser jumping all over the place and mixing up the text I was writing. Once I consulted the handbook, I figured out how turn off the sensitivity by disabling the mouse/right and left click buttons. That, and the sometimes inadvertant click of an FN key that makes something mysterious happen, has probably been my only real problem. As I become more familiar with the laptop, and investigate more of it's potential, I am sure I would write an "excellent" review. I do love the sturdiness of the laptop, and the size is perfect. ps..the one time I had to call the CS line, the CSR was very friendly and helpful.

First laptop

POSTED BY: joe
Overall rating: 4 out of 5 4 out of 5

I like the convenience of the laptop. The only thing that I wish this laptop had was the number keypad along the right side of the keyboard.

Laptop is OK

POSTED BY: Sam1 , Irving,TX
Overall rating: 3 out of 5 3 out of 5

It is a solid laptop and build quality is great. But it has only one USB 2.0 port. You cannot use wireless mouse and USB hard disk at the same time

Go to next laptop

POSTED BY: Griff , Bradenton,FL
Overall rating: 3 out of 5 3 out of 5

If I could have tried it for a month first I would probably not have bought this particular laptop. Even at the cost I paid for this laptop I still would not have bought it.

Good Value

POSTED BY: Suzy , Eliot, ME
Overall rating: 3 out of 5 3 out of 5

All of the wonderful features are overshadowed by the poor battery life. The battery significantly drains while OFF. Nothing more irritating than a laptop you have to keep plugging in! Otherwise it appears to be a great laptop for the money. Performs well...

MSRP: $759.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2310M processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories