Toshiba Satellite S55-A5352 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

a little buggy

POSTED BY: Tarzan , austin, tx
Overall rating: 4 out of 5 4 out of 5

I love the windows 8 format and touch screen, and the operating speed is usually rather good, but it has some pretty annoying problems. the internet stops working randomly and is sometimes rather difficult to fix, the battery gets drained quite a bit in sleep mode compared to my other computers (a day in sleep mode and it dies), it takes a while to save pictures from the internet and will only do this when in desktop view, not windows 8 view. that all said, screen and sound quality are great and there's lots of memory, overall its pretty awesome. now if only I could get rid of this digital keyboard that keeps popping up...

Adequate laptop

POSTED BY: Gardener , IL
Overall rating: 3 out of 5 3 out of 5

First new laptop since 2008 -had a Dell - dislike the Toshiba touchpad - dislike Windows 8 - if I had an opportunity to "try" it before I bought it, I would not have bought it.

MSRP: $699.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S50 shop for accessories