Toshiba Satellite S75-A7270 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Toshiba S75

POSTED BY: RandyN , Puyallup, WA
Overall rating: 4 out of 5 4 out of 5

Overall, I like this laptop a lot. I opted for the larger screen because I mostly use this at home. The screen clarity is excellent. The only complaint I have is the touchpad. I do not like the design of the touchpad. I prefer to have left and right buttons. With this design, I often accidentially move the mouse when trying to do a left or right click. The area of the mouse buttons is a bit too small and makes it harder to use.

Snazzy laptop

POSTED BY: shabuchwae
Overall rating: 4 out of 5 4 out of 5

Looks good, performs well. Nice display, good sound. Not a fan of the touch pad. Love the extra space to the left and right of touch pad. Keyboard is sleek. Slim and light-weight enough. Battery life isn't what I was expecting, and I don't use it heavily when unplugged. Though I think I got my money's worth for this class of laptop.

Good Laptop but poor touchpad

POSTED BY: vicksslc , Salt Lake City, Utah
Overall rating: 3 out of 5 3 out of 5

I would love this laptop if it had touchpad buttons. Instead you only have a sliver of buttons about 1/8 of an inch. If you click out of that area it moves your cursor around so you often make a mistake. Drives me nuts enough that I'm taking it back. I use a touchpad exclusively as I can't use a mouse due to wrist problems. The performance is average. I do a lot of illustrator/photoshop, etc. and this won't cut it. A bit too much lag for my taste. Awesome computer if you're just doing word processing, internet, spreadsheets, etc. - but for designers/video production people - won't cut it. I bought two and taking both back.

MSRP: $749.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3230M Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S70 shop for accessories