Toshiba Satellite S75T-A7160 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great preformer in its price range

POSTED BY: Old goat , Bloomington, MN
Overall rating: 5 out of 5 5 out of 5

Great graphics and other features such as the touch screen. I minor downgraded "features" because of the Windows 8 software. Plays the better games well, although if you use an actual mouse on the right side, the hot air coming out of the vent is annoying on your hand. I use a paper deflector

Quality and Quantity

POSTED BY: AGSizzler , Austin, TX
Overall rating: 5 out of 5 5 out of 5

Best value for the price and has more than enough features. Graphics are great, speed is great. The quad-core processor is lighting fast and the laptop never fails to impress me with all of its features. I don't know if you'll find a better deal than this!

Great Laptop!

POSTED BY: Herculoid62 , Washington, DC
Overall rating: 4 out of 5 4 out of 5

I bought this laptop after it was suggested to me by a close friend who owns a previous model. I was very pleasantly surprised at the performance and all the features it possessed. I added a solid state drive and 8 more gigs of ram and it's moves like lightning. I'm very pleased!

Overall good laptpop

POSTED BY: johnnypo
Overall rating: 4 out of 5 4 out of 5

Display is very nice; boot up speed is very fast. The only minus so far is that it does not have an HDD status LED. I ended up installing a utility that places this status on the toolbar. Otherwise a very nice laptop.

Great except trackpad

POSTED BY: Tekker , Minneapolis, MN
Overall rating: 4 out of 5 4 out of 5

Loved the computer except for the trackpad (which is the only reason it received only 3 stars for performance). Great specs, all-around performance, value. The "tilting" trackpads are a disaster though - the finger slips just slightly when you press for the click, so you slide off of the item you wanted to click on. May not be an issue for some applications, but it was awfully frustrating for me. Returned it and will get another similar model with a conventional track pad.

MSRP: $1049.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8.1
  • 8GB DDR3L 1600MHz memory
  • 2GB DDR3 NVIDIA® GeForce® GT 740M with NVIDIA® Optimus™ technology
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own S70 shop for accessories