Toshiba Satellite S955-S5376 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Good laptop!!

POSTED BY: Bob , Phoenix, AZ
Overall rating: 5 out of 5 5 out of 5

Windows 8 was a barrier for me but when my old laptop died, I had to buy. Glad I did****** This Toshiba satellite was absolutely the best value/performance for the dollar. Windows 8 is different but quite likeable once you understand how to manipulate within the system. The only critique I have of the laptop is the power connector at the computer--it is definitely a weak point in the system. I am very careful when connecting/disconnecting, but if one was to just yank the plug out, you will find yourself with an unusable product. Know it and adapt your behavior accordingly, this laptop is durable and should last a long time. I recommend this laptop to my family and friends.

Great Laptop

POSTED BY: Dutchman , Clinton, CT
Overall rating: 5 out of 5 5 out of 5

Great Laptop great price and great service

Do love except...

POSTED BY: joe , columbia,mo
Overall rating: 5 out of 5 5 out of 5

Learning the start up and shut down was not fast. I went on line to find out if I could shut down faster. There was and other people complained about it as well. Its fixed,so I forgive.

My Second Toshiba

POSTED BY: cathka , Knoxville, TN
Overall rating: 5 out of 5 5 out of 5

I had a problem with my first laptop in that it would not restart when it was turned off or even from hibernation. I began looking at repair costs and decided I would probably pay the same as for a new one and after ordering another brand and it did not work, I returned it and got my second Toshiba. It's dependable, fast and I have no complaints other than Windows 8 which I do not like at all.

opperating system problem

POSTED BY: None , mid minnesota
Overall rating: 3 out of 5 3 out of 5

This is my second Toshiba, very much like the computer! Windows 8 was theft! I had to have windows 8 as it came on the machine, Microsoft took my money for a system that works poorly at best! Support says we can't turn off the hover above what's in setting which does not shut it off! The hover cause's the computer to turn pages and go to links we never intended. Looking on the net MANY! of us are extremely unhappy. I paid for a system that doesn't work, Linux however was free, and it works! Sure would like my money back for windows 8!

Not a good buy ...

POSTED BY: Pzee , FL
Overall rating: 3 out of 5 3 out of 5

If you get a computer and the very next day you are having issues with keyboard and functions of the mouse you better think twice if you want to keep it. I have used Toshiba for many years before I jumped into Macs and tried this one ....

Laptop

POSTED BY: Bill , NC
Overall rating: 3 out of 5 3 out of 5

Poor display and have had display failures with three past Toshiba satellite computers. Too pricey for processer type and installed memory.

MSRP: $749.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3317U Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)