Satellite T135-S1312

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Fantastic little laptop

POSTED BY: toshibanite , South Carolina
Overall rating: 5 out of 5 5 out of 5

It was a toss-up between this and Asus. But for the money this is a great choice. Lots of great features- Keyboard is smooth, Screen size is big enough but still highly portable. The mouse pad buttons could use a better design, but its a small flaw. The sleeper USB is nice to charge device on the go. Get a micro-fiber cloth for the finger prints,and all is well.

Very affordable thin and light laptop

POSTED BY: mark.four , SF, CA
Overall rating: 4 out of 5 4 out of 5

This Toshiba model is a great value for such a light and well designed laptop. Battery life is impressive and it is a very handsome package. I only have two quibbles: the mouse pad is hard to click: I use an external mouse and am much happier. Secondly: the gloss surface shows off all the smudges and fingerprints. Other than that, this is a fine machine in a small package with a great price.

mouse keys are bad

POSTED BY: am
Overall rating: 3 out of 5 3 out of 5

3 complaints: -mousepad keys are terrible. there is one central piece for both keys; you have to press it on the far corners for it to work and it takes too much force to click the buttons. i see this as a major flaw for ease of use. -plastic around monitor feels/looks cheap -fingerprint magnet--even the keys otherwise it seems good. fast so far. haven't used usb charging feature yet, but seems useful.

Not toshibalike

POSTED BY: geeky , chicago, il
Overall rating: 2 out of 5 2 out of 5

I was a little diapaointed in this unit overall. It appears to lack the processing power most laptops in this class have.. No modem so if you are in need of a dialup (in a pinch) you have to find another option. Battery life was less than expected. While I am still a huge Toshiba laptop fan and would not consider another, this one missed the boat.

MSRP: $749.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor SU4100
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 memory
  • 500GB HDD (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories