Satellite U405-S2918

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Portability and Power

POSTED BY: tavo , PERU
Overall rating: 5 out of 5 5 out of 5

Very happy with toshiba and this model. Excellet design and a very light notebook. Good performance for every application I run. Excellent price value.

It's a good machine

POSTED BY: lui , São Carlos, sp, Brasil
Overall rating: 5 out of 5 5 out of 5

This computer is very good, fast and surprising. it lacks to only one s-video input.

Best Laptop Ever

POSTED BY: JJBM
Overall rating: 5 out of 5 5 out of 5

I have been using it for a couple of months now, and it is great!!!. It is nice, really fast, has quite a long battery life, and the price is perfect(very cheap actually) for what you get, which is an amazing laptop.

Good Laptop

POSTED BY: Ashraf , Dubai, United Arab Emirates
Overall rating: 4 out of 5 4 out of 5

It is very nice and intellegent Laptop with new features and abilities, high speed RAM, proccessor, DVD R/W, bluetooth and Wireless LAN, ... etc. but the problem is the battery. battery is less than 2 hours.

good laptop so far!

POSTED BY: tien , chamblee,GA
Overall rating: 4 out of 5 4 out of 5

Nice Laptop

POSTED BY: dempsta , Seattle, WA
Overall rating: 4 out of 5 4 out of 5

Used for a few months everything works as it should. Pros: nice package at nice price, has all the specs I want for home use/small business use. I got the 64 bit vista version and no issues except for trying to find the missing drivers for my printer, etc. Cons: not thrilled about the slick keyboard surface, I touch type and it takes some geting used to. Biggest drag is the bloatware. I wish it were gone. I wish there was a one-click option to uninstall it all. Or provide the bloatware as a CD that you can install as needed.

POSTED BY: bev
Overall rating: 1 out of 5 1 out of 5

It locked up on me often and I returned it. It was a crummy.

MSRP: $979.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor P7450
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories