Satellite U405D-S2874

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

excelent cost great performance

POSTED BY: Abbas zaini , Karbalaa, Iraq
Overall rating: 4 out of 5 4 out of 5

the processor of this computer is one of the most effecient processors nowadays and the ram is really large according to the new needs of OS's , but it misses some very important simple features like the mobile broadband and the bluetooth , but they both can be added externally threw USB and the don't cost much so when you compare it with dell, yes the dell has more features but the price is unaffordable.

Okie-dokie

POSTED BY: tomtom , Honolulu, HI
Overall rating: 4 out of 5 4 out of 5

This laptop was affordable, lightweight, compact, and more. The only thing that I did not like was the batery pack in the back. It sticks out and looks ugly. Also, the laptop becomes really hot compared to my dell and mac laptops.

Worst Laptop Ever

POSTED BY: Jhonny , Bogota
Overall rating: 1 out of 5 1 out of 5

I am fan of toshiba. all my laptops have been toshiba. my last laptop was this laptop and now i am so disappointed whit it.. i don't know why but this computer is so slow, the CPU always works at a 100%. is as bad as it get blocked just playing a song. i can not play a game, i can not play a DVD, i can not use a nice music player, i can not do more than 3 multimedia things.. I'M SO DISSAPOINTED. I really want to know why the people think that this computer is good?. i guess thet the problem is the AMD processor.

Worst laptop ever!!

POSTED BY: Jhonny , Bogota
Overall rating: 1 out of 5 1 out of 5

I'm fan of toshiba laptops.. all my laptops have been toshiba and i use to be happy with it.. but recently i bought this laptop and now i'm so dissapointed with it. i have not used a toshiba pc as bad as this laptop... Is so sloooooooooooooooow. i can't believe that the processor runs at 100% of capacity just playing a song. i can not play a song while i am downloading something from internet because suddenly my computer get blocked. when i'm trying to watch a DVD it looks like an slow-camera. i can not play a geme. I'M SO DISSAPONTED and i want to know why i've this kind of problems. i love Toshiba but i hate my Toshiba U405D.

MSRP: $949.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ X2 Dual-Core Mobile Processor RM-72
  • Windows Vista® Ultimate (64-bit, SP1)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless-LAN (802.11b/g/n)

shop for accessories