Satellite U505-S2970

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My kind of Laptop

POSTED BY: jun , jeddah, saudi arabia
Overall rating: 5 out of 5 5 out of 5

I like it, very nice and really worth your money. Elegant design yet simple, great quality and performance. maybe the screen is too small for me as im using glasses.

U505-S2970

POSTED BY: DIVA
Overall rating: 5 out of 5 5 out of 5

SO FAR I REALLY LIKE THIS LAPTOP... IT IS SLEEK, ELEGANT, AND VERY EASY TO CARRY AROUND. I AM MORE THAN SATISFIED WITH THE COMPONENTS AND ITS SYSTEM. IT WORKS WELL THUS FAR!

Best laptop ever

POSTED BY: cox.nt
Overall rating: 5 out of 5 5 out of 5

Only problem is playback hum when playing music cd

Amazingg!!

POSTED BY: laptopfreaak , Laredo,TX
Overall rating: 5 out of 5 5 out of 5

ive had this comnputer foralready a couple of hours and i already love it the computer doesn't get very hot the battery life is pretty good and i absolutely love the design and features it runs great for now hpe it stays that way.

Awesome laptop!

POSTED BY: mlreccia , Rancho Cucamonga, CA
Overall rating: 5 out of 5 5 out of 5

I love the LED lit keyboard. It is small and stylish. It runs great!

My Satellite

POSTED BY: Ernie , Miami, FL
Overall rating: 4 out of 5 4 out of 5

Excellent laptop! only drawback so far is when opening the Toshiba DVD Player utility, it goes to an error blue screen, after an unstoppable flickering of the screen, and I have to restart the computer every time.very annoying!

bit of a let down

POSTED BY: pwvaf , West Hollywood, CA
Overall rating: 3 out of 5 3 out of 5

The speed and memory are good for the price. However, after having 3 PC laptop with corrupt or malfunctioning hard drives it was recommended I try a Toshiba. Longevity is what I am interested in, and I hope this laptop lives up. Already the H on my keyboard has fallen off after sticking. I imagine I will have to bring it in for repair and be without a computer for several weeks, after just purchasing it. The cursor also tends to jump around randomly while typing. I cannot figure out if this is a programming or keyboard error, as it is inconsistent, with the error.

laptop is OK

POSTED BY: Galina , Encino, CA
Overall rating: 3 out of 5 3 out of 5

For the price this laptop is OK. The keyboard is a little too soft. I tend to hit other keys while typing. My Internet Explorer freezes all the time on this computer, which never happened with others.

MSRP: $899.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor P7450
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 800MHz memory
  • 500GB HDD (5400rpm, Serial ATA)
  • Slot-Loading DVD SuperMulti (+/- Double Layer) with Labelflash®
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories