Toshiba Satellite U945-S4130 Ultrabook

Average Customer Rating:

goes great with check to include
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Go Toshiba!

POSTED BY: Jbbiv , Lakewood WA
Overall rating: 5 out of 5 5 out of 5

I use this for college, I also have online classes using the wifi.

Bad Ops

POSTED BY: the mountainman , central Maryland
Overall rating: 1 out of 5 1 out of 5

This ultrabook is light and portable. that is the good part. the pointing device is way too sensitive, and performs a function sometimes when your hand goes over but does not touch it. And The Worse part of the laptop is Windows 8. what a horrible illogical op system. whoever developed this and the approvers of the system had to be on drugs. The other BAd part is all the useless programs that come pre-installed. why Toshiba, why? And the Toshiba page opens on boot up. Again, why? Give me a real computer where i get to do the thinking instead of the computer guessing what i want and always being wrong. pay the extra and buy a MAC.

terrible wifi

POSTED BY: toshiba user , USA
Overall rating: 1 out of 5 1 out of 5

This laptop has had terrible wifi connections since I bought it 3 months ago. An update to win 8.1 has not helped. It keeps dropping wifi and then is difficult difficult to reconnect. My other computers don't have this problem. My techie friends cannot resolve the issue and I am contacting customer support.

MSRP: $511.49

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3227U Processor
  • Windows 8
  • Intel® Integrated Graphics
  • 500GB HDD (5400 RPM, Serial ATA) with 32GB (system use only) mSATA solid state disk cache
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Intel® Centrino® Wireless-N 2200, 2x2 BGN + Wi-Di Capable