Encore™ Tablet (64GB)

Average Customer Rating:

Free with Purchase!

Toshiba Wireless Speaker v2.1

Toshiba Wireless Speaker v2.1

$99.99 Value


Toshiba recommends Windows.
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Fast, efficient and user-friendly

POSTED BY: Sophie B , Atlanta, GA
Overall rating: 5 out of 5 5 out of 5

Great tablet. This was a gift, but my family knew that I wanted something that has Windows. This has Windows 8. It comes with Microsoft Office and that alone makes it wonderful. It's fast, responsive, and easy to use . This is more of a computer than it is a tablet :-) I consider it a mini-laptop with tablet capabilities.

ba dah da da da im lovin it

POSTED BY: lunnalynn , UT
Overall rating: 3 out of 5 3 out of 5

i love this thing sooo much! although i hate that not many accessories are available right now. I also dislike that not many apps are available. It is glitchy at notifying you if something changes. oh and it is frozen right now... But i do like how i accessible and quick to load everything is. i also love downloading my PowerPoints for school, and that i can continue typing things on the go. however sky drive is slow to update.... i love being able to have two screens open at once and that has definitely come in handy. I think i will eventually become dependent on my tablet but some things like applications and accessories need to become more available.

hdmi out does not work

POSTED BY: hdmi out? , San Francisco, CA
Overall rating: 3 out of 5 3 out of 5

Overall, this tablet is good, love the size as I no longer have to carry a heavy laptop around--or do I? This is the same machine as several other 8" tablets available, but this one is a little heavier. I chose this one primarily for the HDMI out feature, which sadly does not work. The first time I tried using HDMI out, it would only display in Portrait mode. I couldn't get it to flip to landscape. After a number of attempts and reboots, it refused to display anything to the external screen at all. FAIL! Had the HDMI out worked--and worked properly--I would've given this 5 stars but since its unique feature does not work, I can barely eek out 3. The other similar tablets would've been lighter and sleeker.
  • $399.99
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $399.99
  • Free Shipping

add to cart
  • Product summary This product is prebuilt.
  • Windows 8.1
  • Intel® Atom® Processor Z3740 (2MB Cache, Up to 1.86GHz)
  • 2GB LPDDR3 1067MHz -- On board, not user replaceable
  • 64GB eMMC
  • Front 2.0MP Fixed Focus HD Camera
  • Rear 8.0MP Auto Focus HD Camera
  • Micro HDMI® port
  • Micro-USB 2.0
  • Micro SD Card slot
  • Wi-Fi® Wireless networking (802.11a/g/n)
  • Bluetooth® v4.0
  • Sunray Silver
  • 1 Year Standard Limited Warranty
  • Accessories Added: