Please wait...action in progress.
Sorry, Encore™ Tablet (64GB) is not available for sale through Toshibadirect.com. But...
We sell accessories for the Encore™ Tablet (64GB):   
Service Plans Service Plans Other Accessories Other Accessories
We can get you relevant technical support:   
Laptop Forums Product Updates Register Your Product
Downloads and Drivers Locate a Repair Center Technical Support Home
And we can give you details about the Encore™ Tablet (64GB):
Encore™ Tablet (64GB)
Images
IMAGES
 »

Encore™ Tablet (64GB)

  • Windows 8.1
  • Intel® AtomĀ® Processor Z3740 (2MB Cache, Up to 1.86GHz)
  • 2GB LPDDR3 1067MHz -- On board, not user replaceable
  • 64GB eMMC
  • Front 2.0MP Fixed Focus HD Camera
  • Rear 8.0MP Auto Focus HD Camera
  • Micro HDMI® port
  • Micro-USB 2.0
  • Micro SD Card slot
  • Wi-Fi® Wireless networking (802.11a/g/n)
  • Bluetooth® v4.0
  • Sunray Silver
  • 1 Year Standard Limited Warranty
Part Number: PDW09U-002002
Average Customer Rating: 
Read 4 reviews

Questions? Call us at 800-316-0920
Encore™ Tablet (64GB) Encore™ Tablet (64GB)
Rated 4.0/5 based on 4 customer reviews
Product description: Encore™ Tablet (64GB)
 
Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low) »  Rating (low to high) »  Most Recent »  Most Helpful » 

Overall Rating: 5 out of 5 5 out of 5
Fast, efficient and user-friendlyDecember 26, 2013
by Sophie B from Atlanta, GA
Features: 0  out of 5 0 out of 5
Performance: 0 out of 5
Battery Life: 0 out of 5
Price–Value: 0 out of 5
Great tablet. This was a gift, but my family knew that I wanted something that has Windows. This has Windows 8. It comes with Microsoft Office and that alone makes it wonderful. It's fast, responsive, and easy to use . This is more of a computer than it is a tablet :-) I consider it a mini-laptop with tablet capabilities.
What is your level of technical expertise?   TechSavvy
How long have you been using this product?   Less than a week

Overall Rating: 5 out of 5 5 out of 5
Wow! Full featured Pc in a mini tablet!February 20, 2015
by Rusty Hook from New jersey
Features: 0  out of 5 0 out of 5
Performance: 0 out of 5
Battery Life: 0 out of 5
Price–Value: 0 out of 5
This is a zippy little tablet that purchased for work. I have this little dynamo loaded with legacy programs. Microsoft Office enterprise 2007 with a word document open, Excel has a workbook open with 20 sheets using vba and macros, I have a contact manager called Act open, photoshop running with an average size project loaded, and Internet Explorer open, PowerPoint is also running with a large project loaded. When switching between programs, the screens just fly open. I was totally blown away when photoshop cs3 extended installed and ran. Again just one word, Wow!
What is your level of technical expertise?   TechSavvy
How long have you been using this product?   Less than a week

Overall Rating: 3 out of 5 3 out of 5
ba dah da da da im lovin itDecember 12, 2013
by lunnalynn from UT
Features: 0  out of 5 0 out of 5
Performance: 0 out of 5
Battery Life: 0 out of 5
Price–Value: 0 out of 5
i love this thing sooo much! although i hate that not many accessories are available right now. I also dislike that not many apps are available. It is glitchy at notifying you if something changes. oh and it is frozen right now... But i do like how i accessible and quick to load everything is. i also love downloading my PowerPoints for school, and that i can continue typing things on the go. however sky drive is slow to update.... i love being able to have two screens open at once and that has definitely come in handy. I think i will eventually become dependent on my tablet but some things like applications and accessories need to become more available.
What is your level of technical expertise?   ProficientUser
How long have you been using this product?   Less than a week

Overall Rating: 3 out of 5 3 out of 5
hdmi out does not workJanuary 21, 2014
by hdmi out? from San Francisco, CA
Features: 0  out of 5 0 out of 5
Performance: 0 out of 5
Battery Life: 0 out of 5
Price–Value: 0 out of 5
Overall, this tablet is good, love the size as I no longer have to carry a heavy laptop around--or do I? This is the same machine as several other 8" tablets available, but this one is a little heavier. I chose this one primarily for the HDMI out feature, which sadly does not work. The first time I tried using HDMI out, it would only display in Portrait mode. I couldn't get it to flip to landscape. After a number of attempts and reboots, it refused to display anything to the external screen at all. FAIL! Had the HDMI out worked--and worked properly--I would've given this 5 stars but since its unique feature does not work, I can barely eek out 3. The other similar tablets would've been lighter and sleeker.
What is your level of technical expertise?   TechSavvy
How long have you been using this product?   One month to a year
Customer Rating Summary
Encore™ Tablet (64GB)
Averages based on 4 customer reviews
Overall Rating: 4.0 out of 5
Features: 0.0 out of 5
Performance: 0.0 out of 5
Battery Life: 0.0 out of 5
Price–Value: 0.0 out of 5
3 of 4 (75%) customers would recommend this product to a friend.

Encore™ Tablet (64GB) - Write a Review Close  Close

Ultrabook, Celeron, Celeron Inside, Core Inside, Intel, Intel Logo, Intel Atom, Intel Atom Inside, Intel Core, Intel Inside,
Intel Inside Logo, Intel vPro, Pentium, Pentium Inside, vPro Inside, are trademarks of Intel Corporation in the U.S. and/or other countries.