- QR Code Page
- AS3 Troubleshooting
AS3 Troubleshooting
End frequency
Function
The frequency set for [F240: Start frequency] is instantly output at startup.
This parameter is used when the delayed response of starting torque caused by the acceleration/deceleration time affects the frequency.
When the output frequency is decreased to the frequency set for [F243: End frequency], the frequency instantly becomes 0 Hz when stopping.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.