We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
The following V-series related software is available which supports V-series life cycle from system design, degugging, system testing, through operation and maintenance.
The SynchroTrend is an optional software which can be added in the V-series Engineering Tool Ver.2 (V-Tool2). The SynchroTrend can gather the specified user data from V-series cotrollers and save into a file histrically. The data gathering is synchronized with the controller's tasks (SS/HS/MS). Real-time trend graph display is available as well as saved data display. The SynchroTrend supports the testing and commissioning of large systyems effectively.
The New Instrument FB Library is a collection of the function blocks that perform loop controls and sequence operations, which appear frequently in process control applications. By adding this library to the V-series Engineering Tool Ver.2 (V-Tool2), the programming for process control becomes high productivity and reliable.
The New Instrument FB Library has the following features.
The Permissive Fault Diagnosis is an optional software which can be added in the V-series Engineering Tool Ver.2 (V-Tool2). The Permissive Fault Diagnosis analizes the permissive condition (inter-lock circuit) written by LD, and displays the cause signal at the permissive break.
For example, when an auto-run condition is configured by AND/OR logic of many input signals;
Even if the permissive condition is configured by cascade connection of LD networks, this Permissive Fault Diagnosis can track back the networks and show the diagnostic result as a simple LD network.
The Permissive Fault Diagnosis package can make effecitive in system commissioning and troubleshooting.
The Remote Engineering Package can provide remote maintenance environment through Internet. By using the technology of HTTP tunneling and Windows® Remote Desktop, it provides a secure remote maintenance environment without changing the network security policy at the user site.
Main Feature
Operation Environment
Hardware | PC/AT compatible PC (CPU, memory, disk size are not specified. Follow the application's requirements) |
---|---|
Operating System (OS) | Microsoft Windows® XP professional or Windows® server 2003 |
Network Interface Card (NIC) |
2 ports required (1) for connection between application (V-Tool, SCADA) and controllers (2) for connection with Internet access |
Remote Operation Software (RDP) |
Windows® Remote Desktop (included in Windows® XP Professional or Windows® server 2003) |
Remote Controlled Application | V-series Engineering Tool Ver.2 (V-Tool2), or others (out of Toshiba support) |
Network Environment | Any network which can access to Internet (Intranet or Internet) |
Hardware | PC/AT compatible PC (CPU, memory, disk size are not specified. Follow the application's requirements) |
---|---|
Operating System (OS) | Microsoft Windows® XP Home Edition, Windows® XP Professional Edition, Windows® 2000 Professional, or Windows® server 2003 |
Network Interface Card (NIC) |
1 port (for connection with router) |
Remote Operation Software (RDP) |
Windows® Remote Desktop (included in Windows® XP Home Edition, Professional or Windows® server 2003. For other OS, install is possible using Windows® XP setup CD-ROM) |
Network Environment | Network which can access to Internet (Global IP address is necessary) |
The V-Simulator is a software which emulates S3/S2/L3DS controller operation on a PC.
Without using actual controller hardawre, you can test/debug the application program. Therefore it contributes to shorten the application program development and to improve the quality.
Main Features
Hardware | PC/AT compatible PC (CPU, memory, disk size should be followed with V-Tool2/V-Tool3 requirements) |
---|---|
Operating System (OS) | Microsoft Windows® 2000 or Windows® XP |
Network Interface Card (NIC) | Ethernet card is required for Network type |
Support Module | Sequence controller S3 (S3PU45, S3PU55, S3PU65) Sequence controller S2 (S2PU72, S2PU72D, S2PU82) Loop controller L3 (L3PU21) Ethernet module (EN711, EN721, EN731, EN741, EN751A, EN761) Ethernet module (EN611, EN621, EN631, EN641, EN651A, EN661) Ethernet module (FN711) |
* The contents are subject to change without notice for design changes or other reasons.
Let's talk about your customized solutions and packaged deal options. Fill out the form on the right and our product experts will be in touch shortly!