We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

FOR IMMEDIATE RELEASE
Media Contact: Travis Coggin
Toshiba International Corporation
713-466-0277 x3341
TIC-media@toshiba.com

Toshiba Introduces SiC-based Three-Phase Uninterruptible Power Systems Lineup

HOUSTON, TX — June 1, 2015 — Toshiba International Corporation (TIC) today announced its new G2020 Series uninterruptible power system (UPS). The G2020 Series is the latest three-phase UPS designed by Toshiba utilizing silicon carbide (SiC) power modules enabling the UPS to be 98% efficient with 50% load while operating in double-conversion mode.

The G2020 Series UPS utilizes silicon carbide power modules in a three-level design to provide customers with the ultimate in high efficiency power protection. Combining the latest in semiconductor technology with innovative circuit topology and high-performance full digital control ensures the highest level of reliable power quality to meet the demanding needs of the data center industry. With 98.2% efficiency, the highest in the industry for double-conversion UPS, the G2020 produces less heat, noise and interference, lowers cooling costs and saves energy as compared to the conventional UPS, and presents a solution to mission critical infrastructure. The G2020 Series is available in 500 and 750kVA.

“The Toshiba G2020 UPS is the premiere solution for demanding data center applications which require small footprint, high efficiency, and clean uninterruptible power,” said Greg Mack, Vice President and General Manager of the TIC Power Electronics Division. “The G2020, with full digital control, instantaneous waveform control and fast-response current control ensures the highest power quality for all UPS users.”

Jesus Penalver, Product Manager for the TIC Power Electronics Division, added “For redundant high-reliability UPS applications, the Toshiba G2020 excels with a footprint 17% smaller than its G9000 predecessor and up to 57% smaller than competing models. The future of power electronics is SiC power switching technology, with >33% higher junction temperature, higher switching speed, and extremely low switching losses.”

About Toshiba

Toshiba Corporation, a Fortune Global 500 company, channels world-class capabilities in advanced electronic and electrical product and systems into five strategic business domains: Energy & Infrastructure, Community Solutions, Healthcare Systems & Services, Electronic Devices & Components, and Lifestyles Products & Services. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future,” Toshiba promotes global operations towards securing “Growth Through Creativity and Innovation,” and is contributing to the achievement of a world in which people everywhere live in safe, secure and comfortable society.

Founded in Tokyo in 1875, today’s Toshiba is at the heart of a global network of over 590 consolidated companies employing over 200,000 people worldwide, with annual sales surpassing 6.5 trillion yen (US$63 billion).

To find out more about Toshiba, visit www.toshiba.co.jp/index.htm.

About the TIC Power Electronics Division

The TIC Power Electronics division has more than 25 years of experience in uninterruptible power systems. Toshiba produces a versatile range of single-phase and three-phase UPS solutions and accessories hallmarked for outstanding performance and reliability. Single-phase models range from 1 to 22kVA, while three-phase single module systems range from 15 to 1,000kVA, and three-phase parallel module systems from 100 to 8,000kVA. These systems are suitable for a wide range of applications including data centers, telecommunication, retail, healthcare, broadcasting, and industrial.

For more information please visit www.toshibaups.com.

About Toshiba International Corporation

Toshiba International Corporation (TIC) is a Toshiba America Inc. (TAI) Group Company, a wholly owned subsidiary of Toshiba Corporation, and comprised of four divisions - Motors & Drives, Automotive, Power Electronics and Transmission & Distribution. Headquartered in Houston, Texas, TIC provides application solutions to a wide range of industries including general industrial, oil and gas, utilities, datacenters, renewables, HVAC, water/wastewater, and mining. For more information about TIC, please visit www.toshiba.com/tic.

Need a Quote? Have A Question?
x









Processing...
Top Top