We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Support Software

Related Information

The following V-series related software is available which supports V-series life cycle from system design, degugging, system testing, through operation and maintenance.

SynchroTrend --- V-Tool2 add-in software

The SynchroTrend is an optional software which can be added in the V-series Engineering Tool Ver.2 (V-Tool2). The SynchroTrend can gather the specified user data from V-series cotrollers and save into a file histrically. The data gathering is synchronized with the controller's tasks (SS/HS/MS). Real-time trend graph display is available as well as saved data display. The SynchroTrend supports the testing and commissioning of large systyems effectively.

  • Applicable controller: S3PU55B Ver.2.70 or higher
  • Applicable Engineering Tool: Ver.2.6.0 or higher

SynchroTrend image
Click image to enlarge.

To Top

New Instrument FB Library --- V-Tool2 add-in software

The New Instrument FB Library is a collection of the function blocks that perform loop controls and sequence operations, which appear frequently in process control applications. By adding this library to the V-series Engineering Tool Ver.2 (V-Tool2), the programming for process control becomes high productivity and reliable.
The New Instrument FB Library has the following features.

  1. Higher productivity
  2. High-speed processing
  3. Flexible expandability
  4. Reliable code
  • Applicable controller:
    • DS-type: L3PU21 Ver.1.1B or more / L2PU22 Ver.1.18 or higher
    • MCS-type: L1PU11H/12H/LC511/512 Ver.2.23 or more / LC521/522 Ver.2.30 or higher
  • Applicable Engineering Tool: Ver.2.6.1 or higher

New Instrument FB Library image
Click image to enlarge.

To Top

Permissive Fault Diagnosis --- V-Tool2 add-in software

The Permissive Fault Diagnosis is an optional software which can be added in the V-series Engineering Tool Ver.2 (V-Tool2). The Permissive Fault Diagnosis analizes the permissive condition (inter-lock circuit) written by LD, and displays the cause signal at the permissive break.

For example, when an auto-run condition is configured by AND/OR logic of many input signals;

  1. Why auto-run condition is not satisfied ? --- Displays only the cause contacts
  2. Auto-run has been broken. Which is the first fault ? --- Displays the first fault signal

Even if the permissive condition is configured by cascade connection of LD networks, this Permissive Fault Diagnosis can track back the networks and show the diagnostic result as a simple LD network.
The Permissive Fault Diagnosis package can make effecitive in system commissioning and troubleshooting.

  • Applicable controller: S3PU55A/55B Ver.2.76 or higher
  • Applicable controller: S3PU65A Ver.3.78 or higher
  • Applicable Engineering Tool 2: Ver.2.12.0 or higher
  • Applicable Engineering Tool 3: Ver.3.6.0 or higher

To Top

Remote Engineering Package --- Independent package software

The Remote Engineering Package can provide remote maintenance environment through Internet. By using the technology of HTTP tunneling and Windows® Remote Desktop, it provides a secure remote maintenance environment without changing the network security policy at the user site.

Main Feature

  • System integrators can make remote maintenance network worldwide
  • Only Internet connection is required (Port 80 and 443 are used)
  • There is no need to change the firewall
  • Data is encrypted using AES encryption
  • Initial cost and running cost are reasonable

Remote Engineering Package image
Click image to enlarge.

Operation Environment

End-user side PC (to be operated) List
Hardware PC/AT compatible PC
(CPU, memory, disk size are not specified. Follow the application's requirements)
Operating System (OS) Microsoft Windows® XP professional or Windows® server 2003
Network Interface Card
(NIC)
2 ports required
(1) for connection between application (V-Tool, SCADA) and controllers
(2) for connection with Internet access
Remote Operation
Software (RDP)
Windows® Remote Desktop
(included in Windows® XP Professional or Windows® server 2003)
Remote Controlled Application V-series Engineering Tool Ver.2 (V-Tool2),
or others (out of Toshiba support)
Network Environment Any network which can access to Internet
(Intranet or Internet)
System Integrator side PC (to operate) List
Hardware PC/AT compatible PC
(CPU, memory, disk size are not specified. Follow the application's requirements)
Operating System (OS) Microsoft Windows® XP Home Edition, Windows® XP Professional Edition,
Windows® 2000 Professional, or Windows® server 2003
Network Interface Card
(NIC)
1 port (for connection with router)
Remote Operation
Software (RDP)
Windows® Remote Desktop
(included in Windows® XP Home Edition, Professional or Windows® server 2003.
For other OS, install is possible using Windows® XP setup CD-ROM)
Network Environment Network which can access to Internet
(Global IP address is necessary)

To Top

V-Simulator --- Independent package software

The V-Simulator is a software which emulates S3/S2/L3DS controller operation on a PC.
Without using actual controller hardawre, you can test/debug the application program. Therefore it contributes to shorten the application program development and to improve the quality.

Main Features

  • Emulates S3/S2/L3DS operation on a PC. It is the same operation from the V-Tool2/V-Tool3 including execution monitor, data set, etc. (some instructions are not supported)
  • The Windows® API is prepared to access I/O variables. I/O simulation can be available by linking an external application software.
  • V-Simulator supports LAN functionality. The HMI/SCADA can be connected with V-Simulator through network (Ethernet). The communication test can be done.
  • Two types of connection between V-Simulator and V-Tool2/V-Tool3. (1)Stand-alone type which contain both, and (2)Network type using two or more PCs.

V-Simulator image

Operation Environment List
Hardware PC/AT compatible PC
(CPU, memory, disk size should be followed with V-Tool2/V-Tool3 requirements)
Operating System (OS) Microsoft Windows® 2000 or Windows® XP
Network Interface Card (NIC) Ethernet card is required for Network type
Support Module Sequence controller S3 (S3PU45, S3PU55, S3PU65)
Sequence controller S2 (S2PU72, S2PU72D, S2PU82)
Loop controller L3 (L3PU21)
Ethernet module (EN711, EN721, EN731, EN741, EN751A, EN761)
Ethernet module (EN611, EN621, EN631, EN641, EN651A, EN661)
Ethernet module (FN711)
  • TC-net, TOSDIC are registered trademarks of Toshiba Corporation.
  • Other company names and product names herein are trademarks or registered trademarks of the companies concerned.

* The contents are subject to change without notice for design changes or other reasons.

Product Image Gallery

Need a Quote? Have A Question?

Request A Quote

Let's talk about your customized solutions and packaged deal options. Fill out the form on the right and our product experts will be in touch shortly!










Submit
Processing...
Need a Quote? Have A Question?
x









Processing...
Top Top