Selecting how to input run/stop command
Parameter CMOd: Run command select
https://www.toshiba.com/tic/qr/AS3/error?code=CMOd
0: Terminal
Run/stop the inverter with an external ON/OFF signal.
1: Operation panel, Extension panel
Press the [RUN], [STOP] key on the operation panel to run/stop the inverter.
You can do it even on the optional extension panel.
2: Embedded Ethernet
Connect a communication cable to the Ethernet connector 1 or 2, and run/stop the inverter through
the Ethernet communication.
3: RS485 communication (connector 1)
This has the operation panel mounted when shipped from the factory. Remove the operation panel
and connect a communication cable, and you can run/stop the inverter through the RS485 communication.
4: RS485 communication (connector 2)
Connect a communication cable to the RS485 communication connector 2 next to the control terminal block. Then, you can run/stop the inverter through the RS485 communication.
5: Communication option
Run/stop the inverter with a communication option command.
Selecting how to input a frequency command
Parameter FMOd: Frequency command select 1
https://www.toshiba.com/tic/qr/AS3/error?code=FMOd
1: Terminal RR
Analog signal: Input a frequency command with 0 - 10 Vdc.
2: Terminal RX
Analog signal: Input a frequency command with -10 to +10Vdc.
3: Terminal II
Analog signal: Input a frequency command with 4 - 20 mAdc (0 - 20 mAdc).
4: Terminal AI4 (option)
The terminal [AI4] is included in the cassette option. Input a frequency command with an analog signal.
5: Terminal AI5 (option)
The terminal [AI5] is included in the cassette option. Input a frequency command with an analog signal.
10: Touch wheel 1 (power off or press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Even if you turn off the power supply without pressing the [OK] key, a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Even if you turn off the power supply without pressing the [ENT] key, a frequency command value will be saved.
11: Touch wheel 2 (press OK to save)
Use the touch wheel on the operation panel to input a frequency command.
Press the [OK] key, and a frequency command value will be saved.
On the extension panel, use the up and down arrow keys to input a frequency command.
Press the [ENT] key, a frequency command value will be saved.
12: Sr0
Set the value of the parameter [Sr0: Preset speed 0] as a setting value of a frequency command.
15: Terminal Up/Down frequency
Input a frequency command with an Up/Down command to the input terminal.
16: Pulse train
Input a frequency command with a pulse train signal (up to 30 kpps) to the terminals [S4] and [S5].
17: High resolution pulse train (option)
Input a frequency command with a high resolution pulse train signal to the input terminal.
20: Embedded Ethernet
Connect a communication cable to the Ethernet connector 1 or 2, and input a frequency command
through the Ethernet communication.
21: RS485 communication (connector 1)
Remove the operation panel, connect a communication cable, and input a frequency command through the RS485 communication.
22: RS485 communication (connector 2)
Connect a communication cable to the RS485 communication connector 2 next to the control terminal block, and input a frequency command through the RS485 communication.
23: Communication option
Input a frequency command with a communication option command.
Setting Motor overload protection data
Parameter tHrA: Motor overload protection current 1
https://www.toshiba.com/tic/qr/AS3/error?code=tHrA