We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
E-99: Trip for test
Cause:
E-99: Trip for test occurs when an internal test function is executed.
Clearing:
This fault usually occurs intentionally as part of a troubleshooting routine. So long as no issues are apparent with the motor, ASD or driven equipment, you can clear this fault using normal procedures.
Inspect the motor and driven equipment for issues prior to clearing any faults.
Use one of the following methods to clear the fault.
• The [STOP/RESET] button on the AS3 keypad was pressed twice in quick succession
• Activate a digital input that has been programmed to “Reset” function
• Set the tyP (F007) Parameter to: 4: Clear past trips
Discussion
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.