We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
EEP1: EEPROM fault 1
Cause:
EEP1: EEPROM fault 1 occurs when a data write to the ASD EEPROM fails.
Clearing:
Cycle power on the unit. If the fault re-occurs, the unit will need to be serviced or replaced.
Discussion
All of the EEP faults indicate an issue with the ASD EEPROM. These faults will most commonly occur when the EEPROM fails and will need to be replaced.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.