We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Err4: CPU1 fault A

Cause:
ERR4: Control CPU fault typically occurs due to a fault or failure on the ASD internal control CPU.
Clearing:
Cycle power on the unit. If the fault re-occurs, the unit will need to be serviced or replaced. Discussion
Cause:
ERR4: Control CPU fault typically occurs due to a fault or failure on the ASD internal control CPU.
Clearing:
Cycle power on the unit. If the fault re-occurs, the unit will need to be serviced or replaced. Discussion

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top