We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Low-speed signal output frequency
Function
When the output frequency becomes over [F100: Low-speed signal output frequency], the lowspeed signal is output from the output terminal.
• When [F100: Low-speed signal output frequency] is set to "0.0", the ON signal is output when the output frequency is over 0.0 Hz. Therefore, this setting can be used as a running signal.
• This signal can be also used as brake/release signal for the electromagnetic brake.
Output terminal parameter setting
Low-speed signal is the default setting for terminal [R1].
When you want to output the inversion signal (OFF signal), set "5".
• The signals can be also output from the other output terminals depending on the parameter setting.
When you want to output the signals from the relay logic output terminals [FLA]-[FLB]-[FLC], set "4" or "5" for [F132: Terminal FL function]. When you want to output the signals from the terminals [R2A]-[R2C], set "4" or "5" for [F134: Terminal R2 function]. When you want to output the signals from the terminal [FP], set "4" or "5" for [F130: Terminal FP function 1].
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.