We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Reach signal specified frequency
Function
When the output frequency becomes the frequency that is equal to the value for [F101: Reach signal specified frequency] plus or minus the value for [F102: Reach signal detection band], the ON signal (specified frequency attainment signal) is output from a specified output terminal
Output terminal parameter setting
When you want to output the specified frequency attainment signal to the output terminal [FP], set "8" for [F130: Terminal FP function 1].
When you want to output the signal from the relay logic output terminals [FLA]-[FLB]-[FLC], set [F132: Terminal FL function]. When you want to output the signal from the [R1A]-[R1C] terminals, set [F133: Terminal R1 function 1]. When you want to output the signal from the terminals [R2A]-[R2C] set [F134: Terminal R2 function ].
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.