We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Always active function 1

Function

Default settings
By default, the [Always active function 1] parameter will have the [6: Standby] setting selected>.

1.The always active parameter is located under <5. Extended parameters>. Navigate to this option in the settings. Once the <5. Extended parameters> is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F110 Always active function 1].
The [Always active function 1] will keep one of the settings constantly active.
The adjustment range for the [Always active function 1] paramater ranges from 0-177

Click here to view the functions that can be added to this parameter in section 11.8 of the instruction manual.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top