We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Terminal S1 function 1
Function
Default Settings
By default, the [F114 Terminal S1 function 1] parameter will have the [88: Terminal Up frequency] setting selected.
1.The always active function is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F114 Terminal S1 function 1]. Select this function by hitting the [OK] button on the remote.
The [F114 Terminal S1 function 1] will keep one of the settings active.
The adjustment range for the [F114 Terminal S1 function 1] paramater ranges from 0-203.
Depending on which setting you have selected, that specific setting will run accordingly when you close switch R.
For example, when the [F114 Terminal S1 function 1] partamter has the [88: Terminal Up frequency] setting selected, anytime the S1 switch is closed the inverter will run the [88: Terminal Up frequency] command.
Click here to view the functions that can be added to this parameter in section 11.8 of the instruction manual.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.