We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Terminal R1 function 1
Function
Default Settings
By default, the [F133 Terminal R1 function 1] parameter will have the [4: Low speed signal 1] setting selected.
1.The always active function is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F133 Terminal R1 function 1]. Select this function by hitting the [OK] button on the remote.
The [F133 Terminal R1 function] function will turn on a LED that is directly wired to the R1 port from the terminal block.
The adjustment range for the [F133 Terminal R1 function 1] parameter ranges from 0-255.
By default, the [F133 Terminal R1 function 1] parameter will have the [4: Low speed signal 1] setting selected.
Depending on which setting you have selected, that specific setting will force the LED to turn on, depending on the setting you have selected within the parameter.
For example, when the [F132 Terminal FL function 1] parameter has the [4: Low speed signal 1] setting selected, anytime [4: Low speed signal 1] occurs the LED that R1 is connected to will turn on.
Click here to view the functions that can be added to this parameter in section 11.9 of the instruction manual.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.