We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Terminal R function 3
Function
Default Settings
By default, the [F156 Terminal R function 3] parameter will have the [0: No function] setting selected.
1.The [F156 Terminal R function 3] is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F156 Terminal R function 3]. Select this function by hitting the [OK] button on the remote.
4. All functions labeled with a "1" "2" or "3"all will be running at the same time when their corresponding switch is closed.
The adjustment range for the [F156 Terminal R function 3] parameter ranges from 0-203.
Depending on which setting you have selected, that specific setting will force the inverter to perform the selcted setting. The inverter runs all the functions for that specified switch.
For example, when the [F156 Terminal R function 3] parameter has the [0: No function] setting selected, the inverter also checks the function selected for [F112 Terminal R function 1] and [F152 Terminal R function 2] therefor the inverter performs all three functions, since all functions run when the R switch is closed.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.