We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Terminal S1 function 3

Function

Default Settings
By default, the [F158 Terminal S1 function 3] parameter will have the [0: No function] setting selected.
1.The [F158 Terminal S1 function 3] is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [1 Input/Output parameters (F1--)].
3. Next scroll down using the trackpad of the remote until you highlight [F158 Terminal S1 function 3]. Select this function by hitting the [OK] button on the remote.
4. All functions labeled with a "1" "2" or "3"all will be running at the same time when their corresponding switch is closed.
The adjustment range for the [F158 Terminal S1 function 3] parameter ranges from 0-203.
Depending on which setting you have selected, that specific setting will force the inverter to perform the selcted setting. The inverter runs all the functions for that specified switch.
For example, when the [F158 Terminal S1 function 3] parameter has the [0: No function] setting selected, the inverter also checks the function selected for [F114 Terminal RES function 1] and [F154 Terminal RES function 2] therefor the inverter performs all three functions, since all functions run when the S1 switch is closed.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top