We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Frequency command priority select

Function
Default Settings
By default, the [F200 Frequency command priority select] parameter will have the [0: FMod/F207 (switched by TB)] setting selected.

1.The [F200 Freq cmd. Priority select] is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [2 Frequency parameters (F2--)].
3. Next highlight [F200 Freq cmd. Priority select] Select this function by hitting the [OK] button on the remote.

The next thing that will display on the screen is the image displayed above. On the display screen shows two setting types for the [F200 Freq cmd. Priority select] parameter.
1. The first setting shown is [0: FMOd/F207 (switched by TB)]. What this setting entails is that you can switch the frequency from a controller of some type.
2. The second setting is [1: FMOd/F2007 (switched by F208)]. What this setting entails is that the frequency will change once the frequency hits what is it set to hit in F208.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top