We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

RR point 2 frequency

These parameters set the output frequencies for the frequency commands of the analog signals.
You can use the following terminals. The terminals [AI4] and [AI5] are optional.
Voltage input (0 to 10 V) : terminals [RR], [RX], [AI4], and [AI5]
Voltage input (-10 to +10 V) : terminals [RR], [RX], [AI4], and [AI5]
Curret input (4 to 20 mA) : terminals [II], [AI4], and [AI5]
Setting method
Set a frequency command for an analog input amount at two points.
For the corresponding parameters of each terminal and the setting method, refer to the following.
As default setting, the range between the minimum and maximum input amounts is set to 0 to 50.0/60.0 Hz for main analog signal of the terminals. For example, the terminal [RR] is set to 0 to 50.0/60.0 Hz at 0-10 V.
• For the terminal [RX], select the voltage for [F107: Terminal RX input voltage select].
• For the terminal [AI4], select the analog signal for [F148: Terminal AI4 input select]. For the terminal [AI5], select the analog signal for [F149: Terminal AI5 input select]. The terminals [AI4] and [AI5] are optional.
• If noise disturbs stable operation, increase the value for [F209: Analog input filter]. Doing so eliminates the noise of the frequency setting circuit.
• Do not set the same value for point 1 and point 2. Failure to do so displays "Err1".

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top