We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Frequency command select 2

Function

1.The [F207 Freq command select 2] is located under [5. Extended parameters]. Navigate to this option in the settings. Once the [5. Extended parameters] is highlighted select the [OK] button on this option.
2. Next highlight and select the [2 Frequency parameters (F2--)].
3. Next highlight [F207 Freq command select 2] Select this function by hitting the [OK] button on the remote.

This parameter gives the user an option to change the frequency from an external controller that is not already in use.
The [F207 Freq command select 2] ranges from 0-23 different setting options.
The default setting for [F207 Freq command select 2] is [4: Terminal Al4 (option)].

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top