We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Retry
Function:
The inverter is reset automatically when a trip occurs.
A retry usually occurs when these 5 trips occur; Overcurrent, Overvoltage, Overload, Overheat, and Step out (PM only),
During retry, the motor speed search is activated automactically as occasion demands to start a motor smoothly.
During retry, "rtry" is displayed on LCD screen.
The retry counts is cleared (number of retry: 0) after a specified time without occurences of trips from a retry success.
A retry success means that the ouput frequency reaches the frequency command value without tripping.
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.