We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities.
Click here to accept cookies.
TIC's Cookie Policy.
Privacy Policy
Unit of Acc/Dec time
Function
Set a unit of time for acceleration and deceleration.
Unit for a setting time is selected with [F519: Unit of Acc/Dec time].
0: -
1: 0.01s unit (0 after execution)
2: 0.1s unit (0 after execution)
Please reference latest AS3 Instruction Manual more details or latest information.
AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.