We use cookies to support this website, track usage on this website, to perform analytics and to perform promotional activities. Click here to accept cookies.
TIC's Cookie Policy. Privacy Policy

Related Information

Stall prevention level 1

Function:

If the output current exceeds the level set at Stall prevention level 1, stall prevention will automatically lower the output frequency in an attempt to prevent an overcurrent trip.
The default settings for Heavy duty (HD) is 150 and Normal duty (ND) is 120.
100% reference is the inverter rated current.

Please reference latest AS3 Instruction Manual more details or latest information.

AS3 fault codes, descriptions, symptoms and suggested remedies can be found in the below links. Each fault code can also be linked to directly from the AS3 by accessing the QR code on a mobile device while the AS3 is currently experiencing the fault.

Need a Quote? Have A Question?
x









Processing...
Top Top